AM62Ax MCU+ SDK  11.01.00
POK Functions

Introduction

Data Structures

struct  SDL_POK_staticRegs
 POK Static Registers structure. More...
 

Functions

int32_t SDL_POK_enablePP (SDL_PRG_Inst instance, bool enable)
 POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version of the IP. More...
 
int32_t SDL_POK_getStaticRegisters (SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
 POK Function to get the Static Registers. This function reads the values of the static registers such as hysteresis control, voltage detect mode, trim, PORGP and module status. More...
 
int32_t SDL_POK_init (SDL_POK_Inst instance, SDL_POK_config *pConfig)
 POK module configuration API. More...
 
int32_t SDL_POK_verifyConfig (SDL_POK_Inst instance, SDL_POK_config *pConfig)
 POK Function to verify the written configuration. This function checks the provided config against the written config and returns the verification status. More...
 

Function Documentation

◆ SDL_POK_enablePP()

int32_t SDL_POK_enablePP ( SDL_PRG_Inst  instance,
bool  enable 
)

POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version of the IP.

Parameters
instanceInstance of PRG
enableEnable or disable the ping/pong mode
Returns
SDL_PASS for success. SDL Error Code for failure.

◆ SDL_POK_getStaticRegisters()

int32_t SDL_POK_getStaticRegisters ( SDL_POK_Inst  instance,
SDL_POK_staticRegs *  pStaticRegs 
)

POK Function to get the Static Registers. This function reads the values of the static registers such as hysteresis control, voltage detect mode, trim, PORGP and module status.

Parameters
instanceInstance of POK
pStaticRegsPointer to the static registers structure
Returns
SDL_PASS for success. SDL Error Code for Failure.

◆ SDL_POK_init()

int32_t SDL_POK_init ( SDL_POK_Inst  instance,
SDL_POK_config *  pConfig 
)

POK module configuration API.

Parameters
instanceInstance of POK
pConfigPointer to the configuration structure
Returns
SDL_PASS for success. SDL Error Code for Failure.

◆ SDL_POK_verifyConfig()

int32_t SDL_POK_verifyConfig ( SDL_POK_Inst  instance,
SDL_POK_config *  pConfig 
)

POK Function to verify the written configuration. This function checks the provided config against the written config and returns the verification status.

Parameters
instanceInstance of POK
pConfigPointer to the configuration structure
Returns
SDL_PASS if configuration is verified to match. SDL Error Code for Failure.