Provides the APIs for PBIST.
Sub Modules | |
| PBIST Low-Level API | |
Functions | |
| int32_t | SDL_PBIST_selfTest (SDL_PBIST_inst instance, SDL_PBIST_testType testType, uint32_t timeout, bool *pResult) |
| PBIST self test. More... | |
| int32_t | SDL_SBL_PBIST_selfTest (SDL_PBIST_inst instance) |
| PBIST self test for MCU only. More... | |
| uint32_t | SDL_SBL_PBIST_checkDone (SDL_PBIST_inst instance) |
| PBIST API to check if the test is complete. More... | |
| int32_t | SDL_SBL_PBIST_checkResult (SDL_PBIST_inst instance) |
| PBIST API to check if PBIST test is executed successfully. More... | |
Enumerations | |
| enum | SDL_PBIST_inst { SDL_PBIST_INST_MPU, SDL_PBIST_INST_ENCODE, SDL_PBIST_INST_C7X, SDL_PBIST_INST_VPAC, SDL_PBIST_INST_MAIN, SDL_PBIST_INST_MCU } |
| PBIST instance. More... | |
| enum | SDL_PBIST_testType { SDL_PBIST_TEST, SDL_PBIST_NEG_TEST } |
| PBIST self test type. More... | |
Macros | |
| #define | SDL_PBIST_NUM_INSTANCES 6U |
| #define SDL_PBIST_NUM_INSTANCES 6U |
| enum SDL_PBIST_inst |
PBIST instance.
This enum defines the PBIST instances supported by the SDL_PBIST_selfTest API.
| enum SDL_PBIST_testType |
PBIST self test type.
This enum defines the test types supported by the SDL_PBIST_selfTest API.
| int32_t SDL_PBIST_selfTest | ( | SDL_PBIST_inst | instance, |
| SDL_PBIST_testType | testType, | ||
| uint32_t | timeout, | ||
| bool * | pResult | ||
| ) |
PBIST self test.
This function executes a PBIST self test of the specified type for a specific PBIST instance. The test types supported are defined in SDL_PBIST_testType. PBIST is a feature that is used for self test of the memory regions in the SoC. Multiple instances may be supported. Note: The PBIST test is destructive to the cores/IP which are being tested. Therefore it should be executed from a different core than the one under test. It is important to note that execution of PBIST self-tests require preparation of the IPS under test by bringing them to a certain power and reset state before executing the test. The application must take care of this sequence before executing the self-test. The SDL examples give a reference for the necessary sequences. The PBIST instances supported are specific to the SoC, and are defined in the soc-specific header file.
| instance | [IN] PBIST instance |
| testType | [IN] PBIST test type to run. |
| timeout | [IN] Max number of times to check for PBIST done |
| pResult | [OUT] Pointer to variable to indicate result |
| int32_t SDL_SBL_PBIST_selfTest | ( | SDL_PBIST_inst | instance | ) |
PBIST self test for MCU only.
This function executes a PBIST self test of the specified type for a MCU PBIST instance. The test types supported are defined in SDL_PBIST_testType. PBIST is a feature that is used for self test of the memory regions in the SoC. Multiple instances may be supported. Note: The PBIST test is destructive to the cores/IP which are being tested. Therefore it should be executed from a different core than the one under test. It is important to note that execution of PBIST self-tests require preparation of the IPS under test by bringing them to a certain power and reset state before executing the test. The application must take care of this sequence before executing the self-test. The SDL examples give a reference for the necessary sequences. The PBIST instances supported are specific to the SoC, and are defined in the soc-specific header file.
| instance | [IN] PBIST instance |
| uint32_t SDL_SBL_PBIST_checkDone | ( | SDL_PBIST_inst | instance | ) |
PBIST API to check if the test is complete.
This function checks if the PBIST test is complete.
| instance | [IN] PBIST instance |
| int32_t SDL_SBL_PBIST_checkResult | ( | SDL_PBIST_inst | instance | ) |
PBIST API to check if PBIST test is executed successfully.
This function checks if the PBIST test is executed successfully..
| instance | [IN] PBIST instance |