|
AM62Ax MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
39 #ifndef BOOTLOADER_RPRC_H_
40 #define BOOTLOADER_RPRC_H_
48 #include <drivers/soc.h>
49 #include <drivers/hw_include/csl_types.h>
50 #include <drivers/hw_include/cslr_soc.h>
51 #include <drivers/hw_include/soc_config.h>
52 #include <drivers/bootloader/soc/bootloader_soc.h>
53 #include <drivers/bootloader/bootloader_profile.h>
76 #define BOOTLOADER_INVALID_ID ((uint32_t)0xDEADBABE)
81 #define BOOTLOADER_OPMODE_LOCKSTEP (0U)
82 #define BOOTLOADER_OPMODE_STANDALONE (1U)
87 #define BOOTLOADER_MEDIA_MEM ((uint32_t)0xB0070001)
88 #define BOOTLOADER_MEDIA_FLASH ((uint32_t)0xB0070002)
89 #define BOOTLOADER_MEDIA_EMMC ((uint32_t)0xB0070003)
90 #define BOOTLOADER_MEDIA_SD ((uint32_t)0xB0070004)
91 #define BOOTLOADER_MEDIA_BUFIO ((uint32_t)0xB0070005)
92 #define BOOTLOADER_MEDIA_UART ((uint32_t)0xB0070006)
106 typedef struct Bootloader_Params_s
211 typedef struct Bootloader_Fxns_s
225 typedef struct Bootloader_Config_s
237 #include <drivers/bootloader/bootloader_flash.h>
238 #include <drivers/bootloader/bootloader_mem.h>
239 #include <drivers/bootloader/bootloader_buf_io.h>
244 typedef struct Bootloader_CpuInfo_s
257 typedef struct Bootloader_BootImageInfo_s
#define CSL_CORE_ID_MAX
Definition: cslr_soc_defines.h:79
uint32_t coresPresentMap
Definition: bootloader_rprc.h:231
Bootloader_Fxns * fxns
Definition: bootloader_rprc.h:227
uint32_t Bootloader_isCorePresent(Bootloader_Handle handle, uint32_t cslCoreId)
API to check if a particular core's RPRC image is present in the multicore image.
uint32_t memArgsAppImageBaseAddr
Definition: bootloader_rprc.h:108
Bootloader_BootImageInfo bootImageInfo
Definition: bootloader_rprc.h:277
void Bootloader_ReservedMemInit(uint32_t startAddress, uint32_t regionlength)
API to set the memory region of bootloader.
int32_t Bootloader_bootSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
void(* Bootloader_imgCloseFxn)(void *handle, void *args)
Driver implementation to close a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader_rprc.h:192
int32_t Bootloader_rprcImageParseEntryPoint(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Parse entrypoint from RPRC.
uint32_t Bootloader_getBootMedia(Bootloader_Handle handle)
API to get the selected boot media in the bootloader instance.
Bootloader_imgOpenFxn imgOpenFxn
Definition: bootloader_rprc.h:213
void Bootloader_BootImageInfo_init(Bootloader_BootImageInfo *bootImageInfo)
Initialize BootImage info.
@ BOOTLOADER_IMAGE_NOT_LOADED
Definition: bootloader_rprc.h:268
Bootloader_AppImageLoadStatus loadStatus
Definition: bootloader_rprc.h:281
uint32_t bufIoDeviceIndex
Definition: bootloader_rprc.h:117
void Bootloader_Params_init(Bootloader_Params *params)
Initialize Bootloader params.
uint32_t Bootloader_getMulticoreImageSize(Bootloader_Handle handle)
API to fetch the size of the multicore image.
Bootloader_Params bootParams
Definition: bootloader_rprc.h:278
void Bootloader_JumpSelfCpu(void)
API to jump self CPU.
uint32_t rprcOffset
Definition: bootloader_rprc.h:248
void * args
Definition: bootloader_rprc.h:228
Bootloader_imgSeekFxn imgSeekFxn
Definition: bootloader_rprc.h:216
uint8_t * bufIoTempBuf
Definition: bootloader_rprc.h:111
int32_t Bootloader_parseMultiCoreAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse Multicore Appimage.
Bootloader driver configuration, these are filled by SysCfg based on the boot media selected.
Definition: bootloader_rprc.h:226
uint8_t coreId
Definition: bootloader_rprc.h:280
int32_t(* Bootloader_imgCustomFxn)(void *args)
Driver implementation to enable a custom function for a specific bootloader driver - Memory,...
Definition: bootloader_rprc.h:204
uint32_t(* Bootloader_imgOffsetFxn)(void *args)
Driver implementation to get the current offset in the boot media.
Definition: bootloader_rprc.h:165
Bootloader_imgOffsetFxn imgOffsetFxn
Definition: bootloader_rprc.h:215
void Bootloader_close(Bootloader_Handle handle)
Close bootloader driver.
void * socCoreOpMode
Definition: bootloader_rprc.h:233
int32_t Bootloader_bootCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to boot a non-self CPU.
int32_t Bootloader_runCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to run a non-self CPU.
uint32_t bootImageSize
Definition: bootloader_rprc.h:230
Bootloader_AppImageLoadStatus
AppImage load status.
Definition: bootloader_rprc.h:267
int32_t Bootloader_runSelfCpuWithLinux()
API to boot self CPU with Linux.
uint32_t bufIoTempBufSize
Definition: bootloader_rprc.h:114
uint32_t clkHz
Definition: bootloader_rprc.h:247
uint32_t cpuId
Definition: bootloader_rprc.h:246
Data structure containing information related to a particular CPU, required for RPRC loading.
Definition: bootloader_rprc.h:245
int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to load self CPU.
int32_t(* Bootloader_imgOpenFxn)(void *args, Bootloader_Params *params)
Driver implementation to open a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader_rprc.h:139
void Bootloader_powerOffCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to power off a core.
Data structure containing information related all CPUs, this will be filled by Bootloader_parseMultiC...
Definition: bootloader_rprc.h:258
uint32_t bootMedia
Definition: bootloader_rprc.h:229
int32_t Bootloader_runSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
Bootloader_imgCustomFxn imgCustomFxn
Definition: bootloader_rprc.h:218
int32_t Bootloader_rprcImageLoad(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Load application binaries into SOC memory.
void(* Bootloader_imgSeekFxn)(uint32_t location, void *args)
Driver implementation to move read offset on boot media using a specific bootloader driver - Memory,...
Definition: bootloader_rprc.h:179
bool smpEnable
Definition: bootloader_rprc.h:250
Bootloader_imgCloseFxn imgCloseFxn
Definition: bootloader_rprc.h:217
Driver implementation callbacks.
Definition: bootloader_rprc.h:212
void Bootloader_openDma()
API to open DMA channel.
Bootloader_Handle bootHandle
Definition: bootloader_rprc.h:279
int32_t Bootloader_parseAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to Parse Multicore Appimage.
int32_t(* Bootloader_imgReadFxn)(void *dstAddr, uint32_t length, void *args)
Driver implementation to read from boot media using a specific bootloader driver - Memory,...
Definition: bootloader_rprc.h:153
void * Bootloader_Handle
Handle to the Bootloader driver returned by Bootloader_open()
Definition: bootloader_rprc.h:97
uint32_t enableDma
Definition: bootloader_rprc.h:234
void Bootloader_CpuInfo_init(Bootloader_CpuInfo *cpuInfo)
Initialize CPU info.
void Bootloader_closeDma()
API to close DMA channel.
Parameters passed during Bootloader_open()
Definition: bootloader_rprc.h:107
Bootloader_Handle Bootloader_open(uint32_t instanceNum, Bootloader_Params *openParams)
Open bootloader driver.
int32_t Bootloader_loadCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to load a non-self CPU.
uint8_t * scratchMemPtr
Definition: bootloader_rprc.h:232
uintptr_t entryPoint
Definition: bootloader_rprc.h:249
@ BOOTLOADER_IMAGE_LOADED
Definition: bootloader_rprc.h:269
Data structure containing necessary structs to load AppImage on different CPUs.
Definition: bootloader_rprc.h:276
Bootloader_imgReadFxn imgReadFxn
Definition: bootloader_rprc.h:214