- Attention
- See also FreeRTOS, NO RTOS for list of CPU specific supported and unsupported features.
Features Supported
- Register a interrupt callback to a specific CPU number
- Ability to pass user specific argument to the interrupt callback
- Enable, disable, restore and clear specific CPU interrupts
- Enable, disable, restore global CPU interrupt
- For ARM R5,
- Ability to specify interrupt as FIQ or IRQ, level or pulse
- Ability to specify interrupt priority
Features NOT Supported
See also FreeRTOS, NO RTOS for list of unsupported features.
Important Usage Guidelines
- For ARM R5,
- TI VIM is the interrupt controller that is supported.
- HwiP_disable, HwiP_restore, HwiP_enable only affect state of IRQ. FIQ state is not changed
- Refer ARMv7-R Architecture reference manual and SOC TRM for more details.
- On AM62AX,
| CPU type | Valid interrupt numbers | Valid interrupt priorities |
| R5F | 0 .. 511 | 0 (highest) .. 15 (lowest) |
- On C75,
- The C75 CPU supports 64 interrupts.
- The CLEC event ID can be mapped to any of C75 interrupts.
- If you are configuring software interrupt, then set eventId to HWIP_INVALID_EVENT_ID.
- While mapping CLEC event ID to interrupt number, refer the below table and avoid overlapping interrupts.
| Module | Interrupt number used |
| EQEP | 5 .. 7 |
| TIMER | 8 .. 15 |
| I2C | 16 .. 20 |
| GPIO | 21 |
| UART | 22 .. 30 |
| ECAP | 25 .. 27 |
| UDMA | 32 .. 48 |
| EPWM | 49 .. 51 |
| MCASP | 53 .. 58 |
| IPC | 59 .. 62 |
| MCSPI | 1, 2, 31, 52, 63 |
Example Usage
Include the below file to access the APIs,
Example ISR,
void myISR(void *args)
{
}
Example to register a ISR for CPU interrupt 10,
Example to disable and restore interrupts across a crtical section
API
APIs for HW Interrupts