AM62Ax MCU+ SDK  09.01.00

Detailed Description

This file contains:

    WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!

Copyright (C) 2019-2022 Texas Instruments Incorporated - https://www.ti.com/

Declarations for all functions dealing with keywriter

Request message for keywriter

Parameters
hdrstandard TISCI header
image_addr_loLower 32 bit address (in LE format) of the certificate
image_addr_hiHigher 32 bit address (in LE format) of the certificate
key_prog_maskReserved for future use

Data Fields

struct tisci_header hdr
 
uint32_t image_addr_lo
 
uint32_t image_addr_hi
 
uint32_t key_prog_mask [2]
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_keywriter_req::hdr

◆ image_addr_lo

uint32_t tisci_msg_keywriter_req::image_addr_lo

◆ image_addr_hi

uint32_t tisci_msg_keywriter_req::image_addr_hi

◆ key_prog_mask

uint32_t tisci_msg_keywriter_req::key_prog_mask[2]