AM62Ax MCU+ SDK  09.01.00
SDL_LBIST_config_t Struct Reference

Detailed Description

This structure contains the different configuration used for LBIST Note that the LBIST configuration is SOC and instance specific Check SOC documentation for configuration details.



Data Fields

uint32_t dc_def
 
uint32_t divide_ratio
 
uint32_t static_pc_def
 
uint32_t set_pc_def
 
uint32_t reset_pc_def
 
uint32_t scan_pc_def
 
uint64_t prpg_def
 

Field Documentation

◆ dc_def

uint32_t SDL_LBIST_config_t::dc_def

Clock delay after scan_enable switching

◆ divide_ratio

uint32_t SDL_LBIST_config_t::divide_ratio

LBIST clock divide ratio

◆ static_pc_def

uint32_t SDL_LBIST_config_t::static_pc_def

Bitmap of stuck-at patterns to run

◆ set_pc_def

uint32_t SDL_LBIST_config_t::set_pc_def

Bitmap of set patterns to run

◆ reset_pc_def

uint32_t SDL_LBIST_config_t::reset_pc_def

Bitmap of reset patterns to run

◆ scan_pc_def

uint32_t SDL_LBIST_config_t::scan_pc_def

Bitmap of chain test patterns to run

◆ prpg_def

uint64_t SDL_LBIST_config_t::prpg_def

Initial seed for Pseudo Random Pattern generator (PRPG)