This module contains APIs for using the ESM module. The APIs can be used to configure the ESM instances for notification when error events occur and also to set the error pin.
Sub Modules | |
ESM Low-Level API | |
Files | |
file | sdl_esm.h |
This file contains the SDL ESM API's. | |
file | esm/sdl_esm.h |
Header file contains enumerations, structure definitions and function declarations for SDL Error Signaling Module interface. | |
Data Structures | |
struct | SDL_ESM_ErrorConfig_t |
ESM error configuration. More... | |
struct | SDL_ESM_config |
ESM init configuration. More... | |
Functions | |
int32_t | SDL_ESM_getNErrorStatus (SDL_ESM_Inst instance, uint32_t *pStatus) |
SDL ESM API to get the status of the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_getStaticRegisters (SDL_ESM_Inst instance, SDL_ESM_staticRegs *pStaticRegs) |
SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application. More... | |
int32_t | SDL_ESM_verifyConfig (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig) |
SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration. More... | |
int32_t | SDL_ESM_clrNError (SDL_ESM_Inst instance) |
SDL ESM API to clear the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_setNError (SDL_ESM_Inst instance) |
SDL ESM API to set the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_registerECCCallback (SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback eccCallback, void *callbackArg) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application. More... | |
int32_t | SDL_ESM_init (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig, SDL_ESM_applicationCallback applicationCallback, void *appArg) |
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event. More... | |
void | SDL_ESM_hiInterruptHandler (void *arg) |
Esm Hi Interrupt Handler for MCU Esm Instance. More... | |
void | SDL_ESM_loInterruptHandler (void *arg) |
Esm Lo Interrupt Handler for MCU Esm Instance. More... | |
void | SDL_ESM_configInterruptHandler (void *arg) |
Esm Config Interrupt Handler for MCU Instance. More... | |
int32_t | SDL_ESM_getIntNumber (SDL_ESM_Inst esmInstType, SDL_ESM_IntType esmIntType) |
Esm get Interrupt Number corresponding to the input interrupt type. More... | |
Typedefs | |
typedef int32_t | SDL_Result |
typedef int32_t(* | SDL_ESM_applicationCallback) (SDL_ESM_Inst instance, SDL_ESM_IntType intrType, uint32_t grpChannel, uint32_t index, uint32_t intSrc, void *arg) |
Enumerations | |
enum | SDL_ESM_IntType { SDL_ESM_INT_TYPE_HI = 1, SDL_ESM_INT_TYPE_LO = 2, SDL_ESM_INT_TYPE_CFG = 3, SDL_ESM_INT_TYPE_MAX = 4 } |
Macros | |
#define | SDL_ESM_INTNUMBER_INVALID (0xffffffffu) |
Invalid interrupt number. More... | |
#define | SDL_ESM_INST_INVALID (0xfffffffeu) |
Invalid Esm Instance. More... | |
#define | SDL_ESM_ERRORADDR_INVALID (0xffffffffu) |
Address field: Error Address invalid. More... | |
#define | SDL_ESM_ERRORRAMID_INVALID (0xffffffffu) |
Address field: Error RAM ID invalid. More... | |
#define | SDL_ESM_ERRORBITOFFSET_INVALID (0xffffffffffffffffu) |
Address field: Error Bit Error Offset invalid. More... | |
#define | SDL_ESM_ERRORBITGROUP_INVALID (0xffffffffu) |
Address field: Error Bit Error Group invalid. More... | |
#define | SDL_ESM_MAX_EVENT_MAP_NUM_WORDS (32u) |
Maximum number of EVENT words. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_SEC_ERROR (10001u) |
Main MSMC ECC AGGR0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_DED_ERROR (10002u) |
Main MSMC ECC AGGR0 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_SEC_ERROR (10003u) |
Main A72 ECC AGGR0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_DED_ERROR (10004u) |
Main A72 ECC AGGR0 detected 2-bit ECC error source. More... | |
ESM ECC Error source type | |
typedef uint32_t | sdlEsmEccErrorSource_t |
Source of the ECC error which maps to the ESM interrupt source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU0_SEC_ERROR (1u) |
MCU CPU0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU0_DED_ERROR (2u) |
MCU CPU0 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU1_SEC_ERROR (3u) |
MCU CPU1 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU1_DED_ERROR (4u) |
MCU CPU1 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CBASS_SEC_ERROR (5u) |
MCU CBASS detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CBASS_DED_ERROR (6u) |
MCU CBASS detected 2-bit ECC error source. More... | |
#define SDL_ESM_INTNUMBER_INVALID (0xffffffffu) |
#define SDL_ESM_INST_INVALID (0xfffffffeu) |
Invalid Esm Instance.
#define SDL_ESM_ERRORADDR_INVALID (0xffffffffu) |
Address field: Error Address invalid.
#define SDL_ESM_ERRORRAMID_INVALID (0xffffffffu) |
Address field: Error RAM ID invalid.
#define SDL_ESM_ERRORBITOFFSET_INVALID (0xffffffffffffffffu) |
Address field: Error Bit Error Offset invalid.
#define SDL_ESM_ERRORBITGROUP_INVALID (0xffffffffu) |
Address field: Error Bit Error Group invalid.
#define SDL_ESM_MAX_EVENT_MAP_NUM_WORDS (32u) |
Maximum number of EVENT words.
#define SDL_ESM_ECC_PARAM_MCU_CPU0_SEC_ERROR (1u) |
MCU CPU0 detected 1-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MCU_CPU0_DED_ERROR (2u) |
MCU CPU0 detected 2-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MCU_CPU1_SEC_ERROR (3u) |
MCU CPU1 detected 1-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MCU_CPU1_DED_ERROR (4u) |
MCU CPU1 detected 2-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MCU_CBASS_SEC_ERROR (5u) |
MCU CBASS detected 1-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MCU_CBASS_DED_ERROR (6u) |
MCU CBASS detected 2-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_SEC_ERROR (10001u) |
Main MSMC ECC AGGR0 detected 1-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_DED_ERROR (10002u) |
Main MSMC ECC AGGR0 detected 2-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_SEC_ERROR (10003u) |
Main A72 ECC AGGR0 detected 1-bit ECC error source.
#define SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_DED_ERROR (10004u) |
Main A72 ECC AGGR0 detected 2-bit ECC error source.
typedef int32_t SDL_Result |
typedef uint32_t sdlEsmEccErrorSource_t |
Source of the ECC error which maps to the ESM interrupt source.
typedef int32_t(* SDL_ESM_applicationCallback) (SDL_ESM_Inst instance, SDL_ESM_IntType intrType, uint32_t grpChannel, uint32_t index, uint32_t intSrc, void *arg) |
enum SDL_ESM_IntType |
int32_t SDL_ESM_getNErrorStatus | ( | SDL_ESM_Inst | instance, |
uint32_t * | pStatus | ||
) |
SDL ESM API to get the status of the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
pStatus | Pointer to variable to store the status. If status is 1, then error pin is not active. If status is 0, then error pin is active. |
int32_t SDL_ESM_getStaticRegisters | ( | SDL_ESM_Inst | instance, |
SDL_ESM_staticRegs * | pStaticRegs | ||
) |
SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application.
============================================================================
instance | ESM Instance |
pStaticRegs | Pointer to the static config register structure |
int32_t SDL_ESM_verifyConfig | ( | SDL_ESM_Inst | instance, |
const SDL_ESM_config * | pConfig | ||
) |
SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration.
============================================================================
instance | ESM Instance |
pConfig | Pointer to the ESM configuration to be used for verification. |
int32_t SDL_ESM_clrNError | ( | SDL_ESM_Inst | instance | ) |
SDL ESM API to clear the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
int32_t SDL_ESM_setNError | ( | SDL_ESM_Inst | instance | ) |
SDL ESM API to set the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
int32_t SDL_ESM_registerECCCallback | ( | SDL_ESM_Inst | instance, |
uint32_t | eventBitMap[], | ||
SDL_ESM_applicationCallback | eccCallback, | ||
void * | callbackArg | ||
) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application.
============================================================================
instance | ESM Instance |
eventBitMap | Bitmap for ESM error event of interest for this callback. Array of uint32_t type with each bit representing one ESM error event. |
eccCallback | Pointer to the callback to be called by the ESM Handler to notify the ECC module of an ESM error event |
callbackArg | Argument that will be passed along with the callback. |
int32_t SDL_ESM_init | ( | SDL_ESM_Inst | instance, |
const SDL_ESM_config * | pConfig, | ||
SDL_ESM_applicationCallback | applicationCallback, | ||
void * | appArg | ||
) |
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event.
============================================================================
instance | ESM Instance |
pConfig | Pointer to the ESM configuration structure |
applicationCallback | Pointer to the callback to be called by the ESM Handler to notify the application of an ESM error event. |
appArg | Application argument that will passed to the application when the application callback is called. |
void SDL_ESM_hiInterruptHandler | ( | void * | arg | ) |
Esm Hi Interrupt Handler for MCU Esm Instance.
============================================================================
arg | argument for handler |
void SDL_ESM_loInterruptHandler | ( | void * | arg | ) |
Esm Lo Interrupt Handler for MCU Esm Instance.
============================================================================
arg | argument for handler |
void SDL_ESM_configInterruptHandler | ( | void * | arg | ) |
Esm Config Interrupt Handler for MCU Instance.
============================================================================
arg | argument for handler |
int32_t SDL_ESM_getIntNumber | ( | SDL_ESM_Inst | esmInstType, |
SDL_ESM_IntType | esmIntType | ||
) |
Esm get Interrupt Number corresponding to the input interrupt type.
============================================================================
esmInstType | Instance of ESM |
esmIntType | ESM Interrupt type |