AM62Ax MCU+ SDK  09.01.00
APIs for SOC Specific Functions

Introduction

For more details and example usage, see SOC

Functions

int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
uint32_t SOC_getCoreId (const char *coreName)
 Convert a core ID to a user readable name. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
void SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable)
 Enable or disable ePWM time base clock from Control MMR. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
void SOC_unlockAllMMR (void)
 Unlocks all the control MMRs. More...
 
int32_t SOC_moduleGetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)
 Get module clock frequency. More...
 
void SOC_setDevStat (uint32_t bootMode)
 Change boot mode by setting devstat register. More...
 
void SOC_triggerMcuLpmWakeup (void)
 Generates the MCU IPC interrupt to DM R5 to wakeup the main domain from MCU only LPM mode. More...
 
void SOC_generateSwWarmResetMainDomain (void)
 Generate SW Warm Reset Main Domain. More...
 
void SOC_generateSwPORResetMainDomain (void)
 Generate SW POR Reset Main Domain. More...
 
uint32_t SOC_getWarmResetCauseMainDomain (void)
 Get the reset reason source for Main Domain. More...
 
void SOC_generateSwWarmResetMcuDomain (void)
 Generate SW WARM Reset Mcu Domain. More...
 
void SOC_generateSwWarmResetMainDomainFromMcuDomain (void)
 Generate SW WARM Reset Main Domain from Mcu Domain. More...
 
void SOC_generateSwPORResetMainDomainFromMcuDomain (void)
 Generate SW POR Reset Main Domain from Mcu Domain. More...
 
uint32_t SOC_getWarmResetCauseMcuDomain (void)
 Get the reset reason source for Mcu Domain. More...
 
void SOC_clearResetCauseMainMcuDomain (uint32_t resetCause)
 Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason. More...
 
int32_t SOC_enableResetIsolation (uint32_t main2McuIsolation, uint32_t mcu2MainIsolation, uint32_t mcu2dmIsolation, uint32_t debugIsolationEnable)
 Enable reset isolation of MCU domain for safety applications. More...
 
void SOC_setMCUResetIsolationDone (uint32_t value)
 Set MCU reset isolation done flag. More...
 
void SOC_waitMainDomainReset (void)
 Wait for main domain reset to complete. More...
 
int32_t SOC_getPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t *domainState, uint32_t *moduleState)
 Get PSC (Power Sleep Controller) state. More...
 
int32_t SOC_setPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState)
 Set PSC (Power Sleep Controller) state. More...
 

Macros

#define SOC_BOOTMODE_MMCSD   (0X36C3)
 Switch value for SD card boot mode. More...
 

SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 
#define SOC_DOMAIN_ID_MCU   (1U)
 
#define SOC_DOMAIN_ID_WKUP   (2U)
 
#define SOC_PSC_DOMAIN_ID_MAIN   (0U)
 
#define SOC_PSC_DOMAIN_ID_MCU   (1U)
 

SOC PSC Module State

#define SOC_PSC_SYNCRESETDISABLE   (0x0U)
 
#define SOC_PSC_SYNCRESET   (0x1U)
 
#define SOC_PSC_DISABLE   (0x2U)
 
#define SOC_PSC_ENABLE   (0x3U)
 

SOC PSC Domain State

#define SOC_PSC_DOMAIN_OFF   (0x0U)
 
#define SOC_PSC_DOMAIN_ON   (0x1U)
 

Macro Definition Documentation

◆ SOC_DOMAIN_ID_MAIN

#define SOC_DOMAIN_ID_MAIN   (0U)

◆ SOC_DOMAIN_ID_MCU

#define SOC_DOMAIN_ID_MCU   (1U)

◆ SOC_DOMAIN_ID_WKUP

#define SOC_DOMAIN_ID_WKUP   (2U)

◆ SOC_PSC_DOMAIN_ID_MAIN

#define SOC_PSC_DOMAIN_ID_MAIN   (0U)

\ SOC PSC Domain ID

◆ SOC_PSC_DOMAIN_ID_MCU

#define SOC_PSC_DOMAIN_ID_MCU   (1U)

◆ SOC_PSC_SYNCRESETDISABLE

#define SOC_PSC_SYNCRESETDISABLE   (0x0U)

◆ SOC_PSC_SYNCRESET

#define SOC_PSC_SYNCRESET   (0x1U)

◆ SOC_PSC_DISABLE

#define SOC_PSC_DISABLE   (0x2U)

◆ SOC_PSC_ENABLE

#define SOC_PSC_ENABLE   (0x3U)

◆ SOC_PSC_DOMAIN_OFF

#define SOC_PSC_DOMAIN_OFF   (0x0U)

◆ SOC_PSC_DOMAIN_ON

#define SOC_PSC_DOMAIN_ON   (0x1U)

◆ SOC_BOOTMODE_MMCSD

#define SOC_BOOTMODE_MMCSD   (0X36C3)

Switch value for SD card boot mode.

Function Documentation

◆ SOC_moduleClockEnable()

int32_t SOC_moduleClockEnable ( uint32_t  moduleId,
uint32_t  enable 
)

Enable clock to specified module.

Parameters
moduleId[in] see tisci_devices for list of device ID's
enable[in] 1: enable clock to the module, 0: disable clock to the module
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_moduleSetClockFrequency()

int32_t SOC_moduleSetClockFrequency ( uint32_t  moduleId,
uint32_t  clkId,
uint64_t  clkRate 
)

Set module clock to specified frequency.

Parameters
moduleId[in] see tisci_devices for list of module ID's
clkId[in] see tisci_clocks for list of clocks associated with the specified module ID
clkRate[in] Frequency to set in Hz
Returns
SystemP_SUCCESS Module clock is enabled
SystemP_FAILURE Module clock could not be enabled

◆ SOC_getCoreName()

const char* SOC_getCoreName ( uint16_t  coreId)

Convert a core ID to a user readable name.

Parameters
coreId[in] see CSL_CoreID
Returns
name as a string

◆ SOC_getCoreId()

uint32_t SOC_getCoreId ( const char *  coreName)

Convert a core ID to a user readable name.

Parameters
coreName[in] core Name
Returns
coreID

◆ SOC_getSelfCpuClk()

uint64_t SOC_getSelfCpuClk ( void  )

Get the clock frequency in Hz of the CPU on which the driver is running.

Returns
Clock frequency in Hz

◆ SOC_setEpwmTbClk()

void SOC_setEpwmTbClk ( uint32_t  epwmInstance,
uint32_t  enable 
)

Enable or disable ePWM time base clock from Control MMR.

Parameters
epwmInstance[in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)]
enable[in] TRUE to enable and FALSE to disable

◆ SOC_controlModuleLockMMR()

void SOC_controlModuleLockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Lock control module partition to prevent writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_controlModuleUnlockMMR()

void SOC_controlModuleUnlockMMR ( uint32_t  domainId,
uint32_t  partition 
)

Unlock control module partition to allow writes into control MMRs.

Parameters
domainId[in] See SOC_DomainId_t
partition[in] Partition number to unlock

◆ SOC_unlockAllMMR()

void SOC_unlockAllMMR ( void  )

Unlocks all the control MMRs.

◆ SOC_moduleGetClockFrequency()

int32_t SOC_moduleGetClockFrequency ( uint32_t  moduleId,
uint32_t  clkId,
uint64_t *  clkRate 
)

Get module clock frequency.

Parameters
moduleId[in] see tisci_devices for list of module ID's
clkId[in] see tisci_clocks for list of clocks associated with the specified module ID
clkRate[out] Frequency of the clock
Returns
SystemP_SUCCESS on success, else failure

◆ SOC_setDevStat()

void SOC_setDevStat ( uint32_t  bootMode)

Change boot mode by setting devstat register.

Parameters
bootMode[IN] Boot mode switch value

◆ SOC_triggerMcuLpmWakeup()

void SOC_triggerMcuLpmWakeup ( void  )

Generates the MCU IPC interrupt to DM R5 to wakeup the main domain from MCU only LPM mode.

◆ SOC_generateSwWarmResetMainDomain()

void SOC_generateSwWarmResetMainDomain ( void  )

Generate SW Warm Reset Main Domain.

◆ SOC_generateSwPORResetMainDomain()

void SOC_generateSwPORResetMainDomain ( void  )

Generate SW POR Reset Main Domain.

◆ SOC_getWarmResetCauseMainDomain()

uint32_t SOC_getWarmResetCauseMainDomain ( void  )

Get the reset reason source for Main Domain.

Returns
Reset Reason Source Main Domain

◆ SOC_generateSwWarmResetMcuDomain()

void SOC_generateSwWarmResetMcuDomain ( void  )

Generate SW WARM Reset Mcu Domain.

◆ SOC_generateSwWarmResetMainDomainFromMcuDomain()

void SOC_generateSwWarmResetMainDomainFromMcuDomain ( void  )

Generate SW WARM Reset Main Domain from Mcu Domain.

◆ SOC_generateSwPORResetMainDomainFromMcuDomain()

void SOC_generateSwPORResetMainDomainFromMcuDomain ( void  )

Generate SW POR Reset Main Domain from Mcu Domain.

◆ SOC_getWarmResetCauseMcuDomain()

uint32_t SOC_getWarmResetCauseMcuDomain ( void  )

Get the reset reason source for Mcu Domain.

Returns
Reset Reason Source Mcu Domain

◆ SOC_clearResetCauseMainMcuDomain()

void SOC_clearResetCauseMainMcuDomain ( uint32_t  resetCause)

Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason.

Parameters
resetCause[IN] Reset reason value to clear.

◆ SOC_enableResetIsolation()

int32_t SOC_enableResetIsolation ( uint32_t  main2McuIsolation,
uint32_t  mcu2MainIsolation,
uint32_t  mcu2dmIsolation,
uint32_t  debugIsolationEnable 
)

Enable reset isolation of MCU domain for safety applications.

Parameters
main2McuIsolation[IN] Flag to enable isolation of mcu domain from main domain Setting this flag restricts the access of MCU resources by main domain
mcu2MainIsolation[IN] Flag to enable isolation of MCU domain from DM Setting this flag restricts the access of MCU resources by DM
mcu2dmIsolation[IN] Flag to enable isolation of DM from mcu domain Setting this flag restricts the access of DM resources by MCU domain
debugIsolationEnable[IN] Enable debug isolation. Setting this would restrict JTAG access to MCU domain

◆ SOC_setMCUResetIsolationDone()

void SOC_setMCUResetIsolationDone ( uint32_t  value)

Set MCU reset isolation done flag.

Parameters
value[IN] : 0 - Allow main domain reset to propogate : 1 - Do not allow main domain reset to propogate

◆ SOC_waitMainDomainReset()

void SOC_waitMainDomainReset ( void  )

Wait for main domain reset to complete.

◆ SOC_getPSCState()

int32_t SOC_getPSCState ( uint32_t  instNum,
uint32_t  domainNum,
uint32_t  moduleNum,
uint32_t *  domainState,
uint32_t *  moduleState 
)

Get PSC (Power Sleep Controller) state.

Parameters
instNum[IN] : PSC Instance. See SOC_PSCDomainId_t
domainNum[IN] : Power domain number
moduleNum[IN] : Module number
domainState[OUT] : Domain state (1 : ON, 0 : OFF)
moduleState[OUT] : Module State. See SOC_PSCModuleState_t
Returns
SystemP_SUCCESS on success, else failure

◆ SOC_setPSCState()

int32_t SOC_setPSCState ( uint32_t  instNum,
uint32_t  domainNum,
uint32_t  moduleNum,
uint32_t  pscState 
)

Set PSC (Power Sleep Controller) state.

Parameters
instNum[IN] : PSC Instance. See SOC_PSCDomainId_t
domainNum[IN] : Power domain number
moduleNum[IN] : Module number
pscState[IN] : PSC module state. See SOC_PSCModuleState_t
Returns
SystemP_SUCCESS on success, else failure