Return the number of possible parents for a clock.
- Parameters
-
hdr | TISCI header |
device | The device ID that the clock is connected to. |
clk | Each device has its own set of clock inputs. This indexes which clock input to query. |
If the clock index is 255 or greater, this field should be set to 255 and the full value placed in the clk32 field. This is kept for backwards compatibility with older firmwares.
- Parameters
-
clk32 | Stores the actual clock index if clk field is set to 255. This field is ignored otherwise. This field can hold the full range of possible clock indexes, but for compatibility with older firmwares should only be used when the index is 255 or greater. |