Response for retrieving the firewall permissions.
- Parameters
-
hdr | Generic TISCI message header. A ACK response in the hdr indicates that the message was processed. successfully. A NACK response indicates failure to retrieve firewall permissions. |
fwl_id | firewall ID in question. fwl_id is defined in the TRM. |
region | Region or channel number to set config info This field is unused in case of a simple firewall and must be initialized to zero. In case of a region based firewall, this field indicates the region in question. (index starting from 0) In case of a channel based firewall, this field indicates the channel in question (index starting from 0) |
n_permission_regs | Number of permission registers retrieved |
control | Contents of the firewall CONTROL register |
permissions | Contents of the firewall PERMISSION registers |
start_address | Contents of the firewall START_ADDRESS register This is not applicable for channelized firewalls. The returned address is restricted to 44-bit. |
end_address | Contents of the firewall END_ADDRESS register This is not applicable for channelized firewalls. The returned address is restricted to 44-bit. |