AM62Ax MCU+ SDK  09.00.00

Detailed Description

ROM messaging: Payload for loading firmware .

Data Fields

uint32_t bufferAddress
 
uint32_t bufferSizeBytes
 

Field Documentation

◆ bufferAddress

uint32_t Sciclient_RomFirmwareLoadPayload_t::bufferAddress

Address at which the firmware is located

◆ bufferSizeBytes

uint32_t Sciclient_RomFirmwareLoadPayload_t::bufferSizeBytes

Size of firmware. Note : This field is not used read by the ROM. Its value is taken from x509 certificate .