AM62Ax MCU+ SDK  09.00.00
SDL_ECC_staticRegs Struct Reference

Detailed Description

This structure contains the static register group for Ecc aggregator used by the SDL_ecc_aggrReadStaticRegs function.

Design: PROC_SDL-1281

Data Fields

uint32_t REV
 
uint32_t ECC_CTRL
 
uint32_t ECC_ERR_CTRL1
 
uint32_t ECC_ERR_CTRL2
 
uint32_t ECC_SEC_ENABLE_SET_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]
 
uint32_t ECC_SEC_ENABLE_CLR_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]
 
uint32_t ECC_DED_ENABLE_SET_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]
 
uint32_t ECC_DED_ENABLE_CLR_REG [SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]
 

Field Documentation

◆ REV

uint32_t SDL_ECC_staticRegs::REV

Aggregator Revision Register

◆ ECC_CTRL

uint32_t SDL_ECC_staticRegs::ECC_CTRL

ECC Control register

◆ ECC_ERR_CTRL1

uint32_t SDL_ECC_staticRegs::ECC_ERR_CTRL1

ECC Err Control1 register

◆ ECC_ERR_CTRL2

uint32_t SDL_ECC_staticRegs::ECC_ERR_CTRL2

ECC Err Control2 register

◆ ECC_SEC_ENABLE_SET_REG

uint32_t SDL_ECC_staticRegs::ECC_SEC_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]

ECC_SEC_ENABLE_SET_REG registers

◆ ECC_SEC_ENABLE_CLR_REG

uint32_t SDL_ECC_staticRegs::ECC_SEC_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]

ECC_SEC_ENABLE_SET_REG registers

◆ ECC_DED_ENABLE_SET_REG

uint32_t SDL_ECC_staticRegs::ECC_DED_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]

ECC_DED_ENABLE_SET_REG registers

◆ ECC_DED_ENABLE_CLR_REG

uint32_t SDL_ECC_staticRegs::ECC_DED_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS]

ECC_DED_ENABLE_SET_REG registers