AM275 FreeRTOS SDK  12.00.00

Introduction

VTM Driver API/interface file.

Go to the source code of this file.

Macros

#define VTM_TABLE_SIZE   1024
 

Functions

void VTM_printPolynomialLookUpTable ()
 This function is used to print VTM table which defines code values and what temperature value it refers to. More...
 
int32_t VTM_getAverageTemperature (float *temperature)
 This function populates current temperature value. More...
 
void VTM_reset ()
 This function resets the VTM sensors. More...