AM275 FreeRTOS SDK  12.00.00
RTC_HwAttrs Struct Reference

Detailed Description

RTC Hardware attributes.

Data Fields

uint32_t baseAddr
 
uint32_t intNum
 
uint16_t eventId
 
uint32_t inputClk
 
bool enableIntr
 
uint8_t intrPriority
 

Field Documentation

◆ baseAddr

uint32_t RTC_HwAttrs::baseAddr

RTC Peripheral base address

◆ intNum

uint32_t RTC_HwAttrs::intNum

RTC Peripheral interrupt vector

◆ eventId

uint16_t RTC_HwAttrs::eventId

RTC Peripheral event id

◆ inputClk

uint32_t RTC_HwAttrs::inputClk

RTC input clock

◆ enableIntr

bool RTC_HwAttrs::enableIntr

Enable Interrupt

◆ intrPriority

uint8_t RTC_HwAttrs::intrPriority

Interrupt Priority