AM275 FreeRTOS SDK  12.00.00
HYPERBUS_MemTiming Struct Reference

Detailed Description

Register structure for the Memory Timing Register.

Data Fields

uint32_t latency
 
uint32_t writeCSHold
 
uint32_t readCSHold
 
uint32_t writeCSSetup
 
uint32_t readCSSetup
 
uint32_t writeCSHigh
 
uint32_t readCSHigh
 

Field Documentation

◆ latency

uint32_t HYPERBUS_MemTiming::latency

< Initial latency for read/write access, only applicable for HyperRAM CS# hold time for write to CS# deassertion Range 0 to 15 0 means 1 Cycle 15 means 16 Cycles

◆ writeCSHold

uint32_t HYPERBUS_MemTiming::writeCSHold

CS# hold time for read to CS# deassertion Range 0 to 15 0 means 1 Cycle 15 means 16 Cycles

◆ readCSHold

uint32_t HYPERBUS_MemTiming::readCSHold

CS# setup time for write from CS# assertion Range 0 to 15 0 means 1 Cycle 15 means 16 Cycles

◆ writeCSSetup

uint32_t HYPERBUS_MemTiming::writeCSSetup

CS# setup time for read from CS# assertion Range 0 to 15 0 means 1 Cycle 15 means 16 Cycles

◆ readCSSetup

uint32_t HYPERBUS_MemTiming::readCSSetup

CS# high time for write between operations Range 0 to 15 0 means 1.5 Cycle 15 means 16.5 Cycles

◆ writeCSHigh

uint32_t HYPERBUS_MemTiming::writeCSHigh

CS# high time for read between operations Range 0 to 15 0 means 1.5 Cycle 15 means 16.5 Cycles

◆ readCSHigh

uint32_t HYPERBUS_MemTiming::readCSHigh