AM275 FreeRTOS SDK  12.00.00
HYPERBUS_ECCRegions Struct Reference

Detailed Description

ECC region The structure specifies the ECC region start address and size.

Data Fields

uint32_t eccRegionStart0
 
uint32_t eccRegionSize0
 
uint32_t eccRegionStart1
 
uint32_t eccRegionSize1
 
uint32_t eccRegionStart2
 
uint32_t eccRegionSize2
 
uint32_t eccRegionStart3
 
uint32_t eccRegionSize3
 

Field Documentation

◆ eccRegionStart0

uint32_t HYPERBUS_ECCRegions::eccRegionStart0

ECC region-0 start address

◆ eccRegionSize0

uint32_t HYPERBUS_ECCRegions::eccRegionSize0

ECC region-0 size

◆ eccRegionStart1

uint32_t HYPERBUS_ECCRegions::eccRegionStart1

ECC region-1 start address

◆ eccRegionSize1

uint32_t HYPERBUS_ECCRegions::eccRegionSize1

ECC region-1 size

◆ eccRegionStart2

uint32_t HYPERBUS_ECCRegions::eccRegionStart2

ECC region-2 start address

◆ eccRegionSize2

uint32_t HYPERBUS_ECCRegions::eccRegionSize2

ECC region-2 size

◆ eccRegionStart3

uint32_t HYPERBUS_ECCRegions::eccRegionStart3

ECC region-3 start address

◆ eccRegionSize3

uint32_t HYPERBUS_ECCRegions::eccRegionSize3

ECC region-3 size