AM275 FreeRTOS SDK  12.00.00
HYPERBUS_ECCErrorInfo Struct Reference

Detailed Description

ECC Error Information structure.

This structure provides information about the ECC error

Data Fields

uint8_t writeNonAlignError
 
uint8_t singleBitError
 
uint8_t doubleBitError
 

Field Documentation

◆ writeNonAlignError

uint8_t HYPERBUS_ECCErrorInfo::writeNonAlignError

write Non Aligned ECC error

◆ singleBitError

uint8_t HYPERBUS_ECCErrorInfo::singleBitError

One Bit ECC error

◆ doubleBitError

uint8_t HYPERBUS_ECCErrorInfo::doubleBitError

Two Bit ECC error