AM275 FreeRTOS SDK  12.00.00
Enet_IoctlPrms Struct Reference

Detailed Description

Enet IOCTL param.

IOCTL params structure argument for all Enet IOCTL commands

Data Fields

const void * inArgs
 
uint32_t inArgsSize
 
void * outArgs
 
uint32_t outArgsSize
 

Field Documentation

◆ inArgs

const void* Enet_IoctlPrms::inArgs

Pointer to an actual input args struct for the IOCTL cmd

◆ inArgsSize

uint32_t Enet_IoctlPrms::inArgsSize

Size of inArgs structure

◆ outArgs

void* Enet_IoctlPrms::outArgs

Pointer to an actual output args struct for the IOCTL cmd

◆ outArgsSize

uint32_t Enet_IoctlPrms::outArgsSize

Size of outArgs structure