AM275 FreeRTOS SDK  12.00.00

Detailed Description

Output args for CPSW_ALE_IOCTL_GET_PORT_MACADDR command.

Data Fields

CpswAle_MacAddrInfoaddrs
 
uint32_t addrCnt
 
uint32_t totalAddrCnt
 

Field Documentation

◆ addrs

CpswAle_MacAddrInfo* CpswAle_GetPortMacAddrOutArgs::addrs

Application provided buffer populated with MAC addresses reachable on the port number given in inArgs CpswAle_GetPortMacAddrInArgs::portNum

◆ addrCnt

uint32_t CpswAle_GetPortMacAddrOutArgs::addrCnt

Number of MAC entries stored in provided buffer. Will not exceed CpswAle_GetPortMacAddrInArgs::macAddrMax

◆ totalAddrCnt

uint32_t CpswAle_GetPortMacAddrOutArgs::totalAddrCnt

Total number of MAC addresses reachable on given portNum