AM275 FreeRTOS SDK  12.00.00
sdl_vtm.h File Reference

Introduction

This file contains the SDL VTM API's.

Provides the APIs for VTM.

Go to the source code of this file.

Data Structures

struct  SDL_VTM_configVd
 VTM Voltage Domain configuration. More...
 
struct  SDL_VTM_configTs
 VTM temperature sensor configuration. More...
 
struct  SDL_VTM_staticRegsVd
 VTM Static Registers for Voltage Domain. More...
 
struct  SDL_VTM_staticRegsTs
 VTM Static Registers for Temperature sensor. More...
 

Functions

int32_t SDL_VTM_initVd (SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
 VTM Voltage Domain initialization. More...
 
int32_t SDL_VTM_initTs (SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
 VTM Temperature sensor initialization. More...
 
int32_t SDL_VTM_getTemp (SDL_VTM_InstTs instance, uint32_t *pTempVal)
 Read VTM Temperature sensor values in degree celcius. More...
 
int32_t SDL_VTM_getSensorStatus (SDL_VTM_InstTs instance, const SDL_VTM_Stat_read_ctrl *pCtrl, SDL_VTM_Stat_val *pStat_val)
 Read VTM Temperature sensor status. More...
 
int32_t SDL_VTM_intrCntrl (SDL_VTM_InstVd instance, SDL_VTM_intrCtrl intrCtrl)
 Set maximum Threshold values of VTM Temperature sensor. More...
 
int32_t SDL_VTM_verifyConfigVd (SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
 VTM Voltage Domain configures verification. More...
 
int32_t SDL_VTM_verifyConfigTs (SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
 VTM Temperature sensor configures verification. More...
 
int32_t SDL_VTM_getStaticRegistersVd (SDL_VTM_InstVd instance, SDL_VTM_staticRegsVd *pStaticRegs)
 VTM Voltage Domain readback Static configuration registers. More...
 
int32_t SDL_VTM_getStaticRegistersTs (SDL_VTM_InstTs instance, SDL_VTM_staticRegsTs *pStaticRegs)
 VTM Temperature sensor readback Static configuration registers. More...