AM275 FreeRTOS SDK  12.00.00
sdl_r5_utils.h File Reference

Go to the source code of this file.

Functions

uint32_t SDL_UTILS_getCFLR (void)
 
uint32_t SDL_UTILS_getPMOVSR (void)
 
uint32_t SDL_UTILS_getDFSR (void)
 
uint32_t SDL_UTILS_getDFAR (void)
 
uint32_t SDL_UTILS_getIFSR (void)
 
uint32_t SDL_UTILS_getIFAR (void)
 
void SDL_UTILS_enable_event_bus (void)
 

Function Documentation

◆ SDL_UTILS_getCFLR()

uint32_t SDL_UTILS_getCFLR ( void  )

◆ SDL_UTILS_getPMOVSR()

uint32_t SDL_UTILS_getPMOVSR ( void  )

◆ SDL_UTILS_getDFSR()

uint32_t SDL_UTILS_getDFSR ( void  )

◆ SDL_UTILS_getDFAR()

uint32_t SDL_UTILS_getDFAR ( void  )

◆ SDL_UTILS_getIFSR()

uint32_t SDL_UTILS_getIFSR ( void  )

◆ SDL_UTILS_getIFAR()

uint32_t SDL_UTILS_getIFAR ( void  )

◆ SDL_UTILS_enable_event_bus()

void SDL_UTILS_enable_event_bus ( void  )