AM275 FreeRTOS SDK  12.00.00
cb_thread.h File Reference

Introduction

Bindings to POSIX thread, mutex and semaphore functions.

Go to the source code of this file.

Data Structures

struct  cb_tsn_thread_attr_t
 parameters to initialize thread More...
 
struct  cb_waitpoint_t
 Wait points that blocks the execution of a thread at a specific code point until an event occurs. More...
 

Macros

#define CB_TSN_THREAD_NAME_SIZE   128
 data structure for thread attributes More...
 
#define CB_THREAD_T   pthread_t
 
#define CB_THREAD_CREATE(th, attr, func, arg)   pthread_create(th, NULL, func, arg)
 
#define CB_THREAD_JOIN   pthread_join
 
#define CB_THREAD_EXIT   pthread_exit
 
#define CB_THREAD_MUTEX_T   pthread_mutex_t
 
#define CB_THREAD_MUTEX_LOCK   pthread_mutex_lock
 
#define CB_THREAD_MUTEX_TRYLOCK   pthread_mutex_trylock
 
#define CB_THREAD_MUTEX_TIMEDLOCK   pthread_mutex_timedlock
 
#define CB_THREAD_MUTEX_UNLOCK   pthread_mutex_unlock
 
#define CB_THREAD_MUTEX_INIT   pthread_mutex_init
 
#define CB_THREAD_MUTEX_DESTROY   pthread_mutex_destroy
 
#define CB_THREAD_MUTEXATTR_T   pthread_mutexattr_t
 
#define CB_THREAD_MUTEXATTR_INIT   pthread_mutexattr_init
 
#define CB_THREAD_MUTEXATTR_SETPSHARED   pthread_mutexattr_setpshared
 
#define CB_THREAD_PROCESS_SHARED   PTHREAD_PROCESS_SHARED
 
#define CB_THREAD_PROCESS_PRIVATE   PTHREAD_PROCESS_PRIVATE
 
#define CB_THREAD_COND_T   pthread_cond_t
 
#define CB_THREAD_COND_INIT   pthread_cond_init
 
#define CB_THREAD_COND_DESTROY   pthread_cond_destroy
 
#define CB_THREAD_COND_WAIT   pthread_cond_wait
 
#define CB_THREAD_COND_SIGNAL   pthread_cond_signal
 
#define CB_THREAD_COND_BROADCAST   pthread_cond_broadcast
 
#define CB_SEM_T   sem_t
 
#define CB_SEM_INIT   sem_init
 
#define CB_SEM_GETVALUE   sem_getvalue
 
#define CB_SEM_WAIT   sem_wait
 
#define CB_SEM_TRYWAIT   sem_trywait
 
#define CB_SEM_TIMEDWAIT   sem_timedwait
 
#define CB_SEM_POST   sem_post
 
#define CB_SEM_DESTROY   sem_destroy
 
#define CB_SEM_OPEN   sem_open
 
#define CB_SEM_CLOSE   sem_close
 
#define CB_SEM_UNLINK   sem_unlink
 
#define CB_SEM_FAILED   SEM_FAILED
 
#define CB_GETPID   getpid
 
#define cb_waitpoint_wakeup(wp)   CB_THREAD_COND_SIGNAL(&(wp)->condition)
 Wait point wakeup to signal any one thread currently at this wait point. More...
 
#define cb_waitpoint_broadcast(wp)   CB_THREAD_COND_BROADCAST(&(wp)->condition)
 Wait point wakeup to signal all threads currently at this wait point. More...
 
#define cb_waitpoint_lock(wp)   CB_THREAD_MUTEX_LOCK(&(wp)->lock)
 Wait point lock. More...
 
#define cb_waitpoint_unlock(wp)   CB_THREAD_MUTEX_UNLOCK(&(wp)->lock)
 Wait point unlock. More...
 

Functions

static int cb_tsn_thread_attr_init (cb_tsn_thread_attr_t *attr, int pri, int stack_size, const char *name)
 
static int cb_tsn_thread_attr_set_stackaddr (cb_tsn_thread_attr_t *attr, void *stack_addr)
 
static void cb_waitpoint_init (cb_waitpoint_t *wp)
 Wait point initialization. More...
 
static void cb_waitpoint_deinit (cb_waitpoint_t *wp)
 Wait point de-initialization. More...
 
static bool cb_waitpoint_check (cb_waitpoint_t *wp, uint64_t time)
 Wait point check. More...
 
static void cb_waitpoint_wakeup_at (cb_waitpoint_t *wp, uint64_t time, bool dosleep)
 Wait point blocks until wake point has been awoken and after specified time. More...
 
int cb_killproc (int64_t objnum, bool thread_mode)
 kill forcefully running process or thread More...
 
void cb_waitproc (int64_t objnum, bool thread_mode)