AM275-EVM
- Note
- Refer to EVM page for more details on the EVM, TBD
Cable Connections
The figure below shows some important cable connections, ports and switches.
- Take note of the location of the "BOOTMODE" switch, this is used to switch between different boot modes like OSPI, UART, eMMC, SD, NOBOOT mode
- Attention
- Dip Switch (SW9) - MMC0_SEL needs to be selected to switch the interface between eMMC and SD
| MMC0_SELECT | Interface |
| OFF | eMMC |
| ON | SD |
This switch also needs to selected alongside bootmedia switch to select the bootmedia between SD & eMMC
AM275-EVM
Setup UART Terminal
- Attention
- Both JTAG and UART0 is enumerated to same USB port - J17
-
UART2, UART3 and WKUP_UART0 is available from USB port - J22
- Many examples use a standard UART terminal to log the output from the examples. You can use any UART terminal program for the same. Below steps show how to setup the UART terminal from CCS.
- First identify the UART port as enumerated on the host machine.
- Make sure that the EVM and UART cable connected as shown in Cable Connections
- In windows, you can use the "Device Manager" to see the detected UART ports
- Search "Device Manager" in Windows Search Box in the Windows taskbar.
- If dont see any USB serial ports listed in "Device Manager" under "Ports (COM & LPT)", then make sure you have installed the UART to USB driver from FTDI, https://www.ftdichip.com/FTDrivers.htm.
Identify UART Port in Windows Device Manager
- In CCS, goto "View > Console > Serial Console"
UART Terminal Menu
Open New UART Terminal
- Select the UART port, keep other options to default, i.e 115200 baud rate - 8 data bits - No parity - 1 stop bit,
- We use the 1st USB serial port, as seen in the device manager, for below in the SDK
- Flashing application via UART
- Booting application via UART
- Uboot and Linux terminal
- We use the 3rd USB serial port, as seen in the device manager, as terminal output for examples which run from DM R5F (WKUP R5F)
- We use the 4th USB serial port, as seen in the device manager, as terminal output for examples which run from MCU R5F
Connect to UART port
- In this screenshot this happens to be COM27 and COM30. However on your machine this could be different. One tip to make sure there is no mistake in identifying the UART port is to disconnect all other UART to USB devices other than this EVM before checking in device manager.
Flash SOC Initialization Binary
- Attention
- This is a recommended one time step that needs to be done before you can load and run programs via CCS
-
This step needs to be done once unless the OSPI flash has been erased or some other application has been flashed
-
These steps are not applicable for HS-SE devices as JTAG can not be connected to HS-SE devices by default. Follow the steps in Flash an example application for flashing the HS-SE device.
- A quick recap of steps done so far that are needed for the flashing to work
- Make sure the UART port used for terminal is identified as mentioned in Setup UART Terminal
- Make sure python3 is installed as mentioned in Python3
- Make sure you have the EVM power cable and UART cable connected as shown in Cable Connections
- Build all the binaries from the mcu_plus_sdk installation path.
- For Linux
make -sj4 all
- For Windows
gmake -sj4 all
- POWER-OFF the EVM
- Set boot mode to UART BOOTMODE as shown in below image
UART BOOT MODE
- Switch the MMC0_SELECT switch(SW9) to OFF position
MMC INTERFACE SELECT
- POWER-ON the EVM
- You should see character "C" getting printed on the UART terminal every 2-3 seconds as shown below
UART output in UART BOOT MODE
- Close the UART terminal as shown below. This is important, else the UART script in next step wont be able to connect to the UART port.
Close UART terminal
- Note
- For HS-FS device, use sbl_null_hs_fs.cfg as the cfg file.
Flash in progress
- After all the flashing is done, you will see something like below
Flashing successful
- If flashing has failed, see Flash tool error messages and solutions, and resolve the errors.
- If flashing is successful, do the next steps ...
- POWER-OFF the EVM
- Switch the EVM boot mode to OSPI NOR mode as shown below,
OSPI NOR BOOT MODE
- Attention
- If SBL NULL is used for development, GEL files aren't required for R5FSS
BOOT MODE
MMC INTERFACE
Select the MMC interface between eMMC and SD using switch MMC0_SELECT (SW9). This selection also required with bootmedia switch to select the bootmedia between eMMC and SD
| MMC0_SELECT | Interface |
| OFF | eMMC |
| ON | SD |
MMC INTERFACE SELECT
UART BOOT MODE
This mode is used to flash files to the board flash via UART. It can also be used to boot applications via UART.
BOOTMODE [ 8 : 15 ] (SW1) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1101 1100
UART BOOT MODE
OSPI NOR BOOT MODE
This mode is used to boot flashed applications via EVM flash like OSPI NOR flash
BOOTMODE [ 8 : 15 ] (SW1) = 0100 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1100 1110
OSPI BOOT MODE
Fast-xSPI BOOT MODE
This mode is used to boot flashed applications via EVM flash like OSPI NOR flash in Fast-xSPI mode
BOOTMODE [ 8 : 15 ] (SW1) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1101 0110
Fast-xSPI BOOT MODE
SD BOOT MODE
This mode is used to boot applications via SD card on the EVM.
BOOTMODE [ 8 : 15 ] (SW1) = 0100 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1100 0010
SD BOOT MODE
NOBOOT MODE
BOOTMODE [ 8 : 15 ] (SW1) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1101 1111
NO BOOT MODE
DEVBOOT MODE
BOOTMODE [ 8 : 15 ] (SW1) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1101 1110
DEV BOOT MODE
EMMC BOOT MODE
This mode is used to boot applications via eMMC on the EVM.
BOOTMODE [ 8 : 15 ] (SW1) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1101 0011
EMMC BOOT MODE
Troubleshooting EVM issues
- JTAG connection fails on some EVMs with the following error. Need to connect the JTAG cable after board is powered on.
JTAG Connection Error Dialog