Structure containing R5F CPU Static Registers.
Design: PROC_SDL-6331
Data Fields | |
uint32_t | MIDR |
uint32_t | CTR |
uint32_t | TCMTR |
uint32_t | MPUIR |
uint32_t | MPIDR |
uint32_t | PFR0 |
uint32_t | PFR1 |
uint32_t | ID_DFR0 |
uint32_t | ID_AFR0 |
uint32_t | ID_MMFR0 |
uint32_t | ID_MMFR1 |
uint32_t | ID_MMFR2 |
uint32_t | ID_MMFR3 |
uint32_t | ID_ISAR0 |
uint32_t | ID_ISAR1 |
uint32_t | ID_ISAR2 |
uint32_t | ID_ISAR3 |
uint32_t | ID_ISAR4 |
uint32_t | ID_ISAR5 |
uint32_t | CCSIDR |
uint32_t | CLIDR |
uint32_t | AIDR |
uint32_t | CSSELR |
uint32_t | SCTLR |
uint32_t | ACTLR |
uint32_t | SecondaryACTLR |
uint32_t | CPACR |
uint32_t | MPURegionBaseADDR |
uint32_t | MPURegionEnableR |
uint32_t | MPURegionAccessControlR |
uint32_t | RGNR |
uint32_t | BTCMRegionR |
uint32_t | ATCMRegionR |
uint32_t | SlavePortControlR |
uint32_t | CONTEXTIDR |
uint32_t | ThreadProcessIDR1 |
uint32_t | ThreadProcessIDR2 |
uint32_t | ThreadProcessIDR3 |
uint32_t | nVALIRQSET |
uint32_t | nVALFIQSET |
uint32_t | nVALRESETSET |
uint32_t | nVALDEBUGSET |
uint32_t | nVALIRQCLEAR |
uint32_t | nVALFIQCLEAR |
uint32_t | nVALRESETCLEAR |
uint32_t | nVALDEBUGCLEAR |
uint32_t | BuildOption1R |
uint32_t | BuildOption2R |
uint32_t | PinOptionR |
uint32_t | LLPPnormalAXIRR |
uint32_t | LLPPvirtualAXIRR |
uint32_t | AHBRR |
uint32_t | CFLR |
uint32_t | PMOVSR |
uint32_t | DFSR |
uint32_t | ADFSR |
uint32_t | DFAR |
uint32_t | IFSR |
uint32_t | IFAR |
uint32_t | AIFSR |
uint32_t SDL_R5FCPU_StaticRegs::MIDR |
uint32_t SDL_R5FCPU_StaticRegs::CTR |
uint32_t SDL_R5FCPU_StaticRegs::TCMTR |
uint32_t SDL_R5FCPU_StaticRegs::MPUIR |
uint32_t SDL_R5FCPU_StaticRegs::MPIDR |
uint32_t SDL_R5FCPU_StaticRegs::PFR0 |
uint32_t SDL_R5FCPU_StaticRegs::PFR1 |
uint32_t SDL_R5FCPU_StaticRegs::ID_DFR0 |
uint32_t SDL_R5FCPU_StaticRegs::ID_AFR0 |
uint32_t SDL_R5FCPU_StaticRegs::ID_MMFR0 |
uint32_t SDL_R5FCPU_StaticRegs::ID_MMFR1 |
uint32_t SDL_R5FCPU_StaticRegs::ID_MMFR2 |
uint32_t SDL_R5FCPU_StaticRegs::ID_MMFR3 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR0 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR1 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR2 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR3 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR4 |
uint32_t SDL_R5FCPU_StaticRegs::ID_ISAR5 |
uint32_t SDL_R5FCPU_StaticRegs::CCSIDR |
uint32_t SDL_R5FCPU_StaticRegs::CLIDR |
uint32_t SDL_R5FCPU_StaticRegs::AIDR |
uint32_t SDL_R5FCPU_StaticRegs::CSSELR |
uint32_t SDL_R5FCPU_StaticRegs::SCTLR |
uint32_t SDL_R5FCPU_StaticRegs::ACTLR |
uint32_t SDL_R5FCPU_StaticRegs::SecondaryACTLR |
uint32_t SDL_R5FCPU_StaticRegs::CPACR |
uint32_t SDL_R5FCPU_StaticRegs::MPURegionBaseADDR |
uint32_t SDL_R5FCPU_StaticRegs::MPURegionEnableR |
uint32_t SDL_R5FCPU_StaticRegs::MPURegionAccessControlR |
uint32_t SDL_R5FCPU_StaticRegs::RGNR |
uint32_t SDL_R5FCPU_StaticRegs::BTCMRegionR |
uint32_t SDL_R5FCPU_StaticRegs::ATCMRegionR |
uint32_t SDL_R5FCPU_StaticRegs::SlavePortControlR |
uint32_t SDL_R5FCPU_StaticRegs::CONTEXTIDR |
uint32_t SDL_R5FCPU_StaticRegs::ThreadProcessIDR1 |
uint32_t SDL_R5FCPU_StaticRegs::ThreadProcessIDR2 |
uint32_t SDL_R5FCPU_StaticRegs::ThreadProcessIDR3 |
uint32_t SDL_R5FCPU_StaticRegs::nVALIRQSET |
uint32_t SDL_R5FCPU_StaticRegs::nVALFIQSET |
uint32_t SDL_R5FCPU_StaticRegs::nVALRESETSET |
uint32_t SDL_R5FCPU_StaticRegs::nVALDEBUGSET |
uint32_t SDL_R5FCPU_StaticRegs::nVALIRQCLEAR |
uint32_t SDL_R5FCPU_StaticRegs::nVALFIQCLEAR |
uint32_t SDL_R5FCPU_StaticRegs::nVALRESETCLEAR |
uint32_t SDL_R5FCPU_StaticRegs::nVALDEBUGCLEAR |
uint32_t SDL_R5FCPU_StaticRegs::BuildOption1R |
uint32_t SDL_R5FCPU_StaticRegs::BuildOption2R |
uint32_t SDL_R5FCPU_StaticRegs::PinOptionR |
uint32_t SDL_R5FCPU_StaticRegs::LLPPnormalAXIRR |
uint32_t SDL_R5FCPU_StaticRegs::LLPPvirtualAXIRR |
uint32_t SDL_R5FCPU_StaticRegs::AHBRR |
uint32_t SDL_R5FCPU_StaticRegs::CFLR |
uint32_t SDL_R5FCPU_StaticRegs::PMOVSR |
uint32_t SDL_R5FCPU_StaticRegs::DFSR |
uint32_t SDL_R5FCPU_StaticRegs::ADFSR |
uint32_t SDL_R5FCPU_StaticRegs::DFAR |
uint32_t SDL_R5FCPU_StaticRegs::IFSR |
uint32_t SDL_R5FCPU_StaticRegs::IFAR |
uint32_t SDL_R5FCPU_StaticRegs::AIFSR |