Parameters used to register the ESM notify function to handle Group1 and Group2 errors. The notify function will be invoked post the ESM FIQ interrupt handler processing.
Data Fields | |
uint32_t | groupNumber |
uint32_t | errorNumber |
uint32_t | setIntrPriorityLvl |
bool | enableInfluenceOnErrPin |
void * | arg |
SDL_ESM_CallBack | callBackFunction |
SDL_ESM_ErrorConfig_t | esmErrorConfig |
uint32_t SDL_ESM_NotifyParams::groupNumber |
Group number to which the following error number belongs.
uint32_t SDL_ESM_NotifyParams::errorNumber |
Error number for which the notify function is registered.
uint32_t SDL_ESM_NotifyParams::setIntrPriorityLvl |
Set the interrupt priority level to high or low. Applicable to Group 1 errors only.
bool SDL_ESM_NotifyParams::enableInfluenceOnErrPin |
Enable failure influence on ERROR pin. Applicable to Group 1 errors only.
void* SDL_ESM_NotifyParams::arg |
Argument passed back when the Notify function is invoked.
SDL_ESM_CallBack SDL_ESM_NotifyParams::callBackFunction |
Notify function called by the ESM Module.
SDL_ESM_ErrorConfig_t SDL_ESM_NotifyParams::esmErrorConfig |
Error event to be used for self test