Structure defining the pin configuration parameters.
Data Fields | |
uint32_t | offset |
uint32_t | settings |
uint32_t Pinmux_PerCfg_t::offset |
Register offset for configuring the pin. Refer Pinmux_Offsets. Set this to PINMUX_END to demark the end of configuration array
uint32_t Pinmux_PerCfg_t::settings |
Value to be configured. Active mode configurations like mux mode, pull resistor and buffer mode.
To set a value use like : "| PIN_PULL_DISABLE" To reset a value use like : "& (~PIN_PULL_DIRECTION)"
For example, PIN_MODE(7) | ((PIN_PULL_DISABLE | PIN_INPUT_ENABLE) & (~PIN_PULL_DIRECTION)