MIBSPI peripheral profile Parameters.
When MIBSPI is configured as controller mode, it may connect to multiple peripherals. This data structure captures the the configurations for remote peripherals.
Data Fields | |
| uint8_t | chipSelect |
| uint8_t | ramBufLen |
| uint32_t | dmaReqLine |
| uint8_t MIBSPI_PeripheralProfile::chipSelect |
CS0-CS7 signal number from 0 -7
| uint8_t MIBSPI_PeripheralProfile::ramBufLen |
RAM Length in bytes that used by the peripheral
| uint32_t MIBSPI_PeripheralProfile::dmaReqLine |
DMA request line to be used for peripheral