Data Fields | |
| Icssg_MdioLinkStateChangeCb | mdioLinkStateChangeCb |
| void * | mdioLinkStateChangeCbArg |
| const PRUICSS_IntcInitData * | prussIntcInitData |
| int32_t | coreIntrNum |
| uint32_t | pruEvtNum [ICSSG_MAC_PORT_MAX] |
| uint32_t | isPulseIntr |
| uint32_t | intrPrio |
| Icssg_MdioLinkStateChangeCb Icssg_mdioLinkIntCfg::mdioLinkStateChangeCb |
MDIO Link state change callback function pointer
| void* Icssg_mdioLinkIntCfg::mdioLinkStateChangeCbArg |
Application data to be passed to the MDIO link state change callback
| const PRUICSS_IntcInitData* Icssg_mdioLinkIntCfg::prussIntcInitData |
INTC Module mapping data passed by application for configuring PRU to R5F interrupts
| int32_t Icssg_mdioLinkIntCfg::coreIntrNum |
| uint32_t Icssg_mdioLinkIntCfg::pruEvtNum[ICSSG_MAC_PORT_MAX] |
| uint32_t Icssg_mdioLinkIntCfg::isPulseIntr |
| uint32_t Icssg_mdioLinkIntCfg::intrPrio |