AM273x MCU+ SDK  09.02.00
FirewallRegionReq_t Struct Reference

Detailed Description

This is a FirewallRegionReq type which holds the information of Firewall region configuration.

Data Fields

uint16_t firewallId
 
uint16_t region
 
uint32_t permissionAttributes
 
uint32_t startAddress
 
uint32_t endAddress
 

Field Documentation

◆ firewallId

uint16_t FirewallRegionReq_t::firewallId

Index of the firewall.

◆ region

uint16_t FirewallRegionReq_t::region

Region number

◆ permissionAttributes

uint32_t FirewallRegionReq_t::permissionAttributes

Memory Protection Permission Attributes corresponding to the firewall

◆ startAddress

uint32_t FirewallRegionReq_t::startAddress

Start Address of the region

◆ endAddress

uint32_t FirewallRegionReq_t::endAddress

End Address of the region