Enet IOCTL param.
IOCTL params structure argument for all Enet IOCTL commands
Data Fields | |
| const void * | inArgs |
| uint32_t | inArgsSize |
| void * | outArgs |
| uint32_t | outArgsSize |
| const void* Enet_IoctlPrms::inArgs |
Pointer to an actual input args struct for the IOCTL cmd
| uint32_t Enet_IoctlPrms::inArgsSize |
Size of inArgs structure
| void* Enet_IoctlPrms::outArgs |
Pointer to an actual output args struct for the IOCTL cmd
| uint32_t Enet_IoctlPrms::outArgsSize |
Size of outArgs structure