Timestamp set.
Data Fields | |
| uint64_t | tsLoadVal |
| uint8_t | clkMode |
| uint8_t | clkSign |
| uint64_t EnetTimeSync_setTimestamp::tsLoadVal |
timestamp value in nano seconds unit to set
| uint8_t EnetTimeSync_setTimestamp::clkMode |
mode of the clock. Applicable only to ICSSG peripheral. Says whether given value tsLoadVal is absolute or related. 0: absolute, 1: relative
| uint8_t EnetTimeSync_setTimestamp::clkSign |