Config state machine variables. See IEEE Std 802.1Q-2018 8.6.8.4.
Data Fields | |
| uint64_t | configChangeTime |
| uint32_t | configChangeErrorCounter |
| uint8_t | configPending |
| uint8_t | configChange |
| uint64_t EnetTas_ConfigStatus::configChangeTime |
New list is copied at this time.
| uint32_t EnetTas_ConfigStatus::configChangeErrorCounter |
Config change error counter, incremented if admin->baseTime < current time and TAS_enabled is true.
| uint8_t EnetTas_ConfigStatus::configPending |
True if list update is pending.
| uint8_t EnetTas_ConfigStatus::configChange |
Set to true when application trigger updating of admin list to active list, cleared when configChangeTime is updated.