Priority map.
It can be used for priority regeneration as well as for QoS egress priority remapping.
Data Fields | |
| uint32_t | priorityMap [ENET_PRI_NUM] |
| uint32_t EnetPort_PriorityMap::priorityMap[ENET_PRI_NUM] |
Packet priority map. Map index is the input priority, map value is the output priority.