PHY State-Machine time-out values.
Data Fields | |
| uint32_t | findingStateTicks |
| FINDING state timeout (in ticks). More... | |
| uint32_t | resetWaitStateTicks |
| RESET_WAIT state timeout (in ticks). More... | |
| uint32_t | resetWaitStateResidenceTicks |
| RESET_WAIT state residence time (in ticks). More... | |
| uint32_t | nwayStartStateTicks |
| NWAY_START state timeout (in ticks). More... | |
| uint32_t | nwayWaitStateTicks |
| NWAY_WAIT state timeout (in ticks). More... | |
| uint32_t | linkWaitStateTicks |
| LINK_WAIT state timeout (in ticks). More... | |
| uint32_t | mdixTicks |
| Timeout if MDIX is enabled (in ticks). More... | |
| uint32_t EnetPhy_FsmTimeoutCfg::findingStateTicks |
FINDING state timeout (in ticks).
Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately
| uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateTicks |
RESET_WAIT state timeout (in ticks).
Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately
| uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateResidenceTicks |
RESET_WAIT state residence time (in ticks).
| uint32_t EnetPhy_FsmTimeoutCfg::nwayStartStateTicks |
NWAY_START state timeout (in ticks).
Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately
| uint32_t EnetPhy_FsmTimeoutCfg::nwayWaitStateTicks |
NWAY_WAIT state timeout (in ticks).
Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately
| uint32_t EnetPhy_FsmTimeoutCfg::linkWaitStateTicks |
LINK_WAIT state timeout (in ticks).
Set to ENETPHY_TIMEOUT_WAIT_FOREVER, to disable timeout.
Set to ENETPHY_TIMEOUT_NO_WAIT, to expire immediately
| uint32_t EnetPhy_FsmTimeoutCfg::mdixTicks |
Timeout if MDIX is enabled (in ticks).