Ethernet Module object.
Data Fields | |
| const char * | name |
| uint64_t | physAddr |
| void * | virtAddr |
| uint64_t | physAddr2 |
| void * | virtAddr2 |
| uint32_t | features |
| uint32_t | errata |
| Enet_Magic | magic |
| EnetMod_Open | open |
| EnetMod_Rejoin | rejoin |
| EnetMod_Ioctl | ioctl |
| EnetMod_Close | close |
| EnetMod_SaveCtxt | saveCtxt |
| EnetMod_RestoreCtxt | restoreCtxt |
| const char* EnetMod_Obj::name |
Module name
| uint64_t EnetMod_Obj::physAddr |
Module's physical address
| void* EnetMod_Obj::virtAddr |
Module's virtual address
| uint64_t EnetMod_Obj::physAddr2 |
Module's second physical address, if needed
| void* EnetMod_Obj::virtAddr2 |
Module's second virtual address, if needed
| uint32_t EnetMod_Obj::features |
Module features
| uint32_t EnetMod_Obj::errata |
Module's applicable errata
| Enet_Magic EnetMod_Obj::magic |
Magic number indicating if the module has been opened
| EnetMod_Open EnetMod_Obj::open |
Pointer to the EnetMod open function
| EnetMod_Rejoin EnetMod_Obj::rejoin |
Pointer to the EnetMod rejoin function
| EnetMod_Ioctl EnetMod_Obj::ioctl |
Pointer to the EnetMod ioctl function
| EnetMod_Close EnetMod_Obj::close |
Pointer to the EnetMod close function
| EnetMod_SaveCtxt EnetMod_Obj::saveCtxt |
Pointer to the EnetMod saveCtxt function
| EnetMod_RestoreCtxt EnetMod_Obj::restoreCtxt |
Pointer to the EnetMod restoreCtxt function