Input args for ENET_MDIO_IOCTL_C45_READ command.
Clause-45 register read arguments.
Data Fields | |
| EnetMdio_Group | group |
| uint32_t | phyAddr |
| EnetMdio_C45Mmd | mmd |
| uint16_t | reg |
| EnetMdio_Group EnetMdio_C45ReadInArgs::group |
User channel to be used to perform the register access. Simultaneous access from same group is not allowed. Not applicable in manual mode.
| uint32_t EnetMdio_C45ReadInArgs::phyAddr |
PHY address
| EnetMdio_C45Mmd EnetMdio_C45ReadInArgs::mmd |
MMD
| uint16_t EnetMdio_C45ReadInArgs::reg |
Register address