Input args for ENET_MDIO_IOCTL_C22_WRITE command.
Clause-22 register write arguments.
Data Fields | |
| EnetMdio_Group | group |
| uint32_t | phyAddr |
| uint16_t | reg |
| uint16_t | val |
| EnetMdio_Group EnetMdio_C22WriteInArgs::group |
User channel to be used to perform the register access. Simultaneous access from same group is not allowed. Not applicable in manual mode.
| uint32_t EnetMdio_C22WriteInArgs::phyAddr |
PHY address
| uint16_t EnetMdio_C22WriteInArgs::reg |
Register address
| uint16_t EnetMdio_C22WriteInArgs::val |
Value to be written