AM273x MCU+ SDK  09.02.00
EfuseRowWrite_t Struct Reference

Detailed Description

This is a EfuseRowWrite type which holds the information regarding programming eFuse row.

Data Fields

uint32_t rowData
 
uint32_t rowBitMask
 
uint8_t rowIdx
 
uint8_t rsvd [3]
 

Field Documentation

◆ rowData

uint32_t EfuseRowWrite_t::rowData

◆ rowBitMask

uint32_t EfuseRowWrite_t::rowBitMask

Data to be written in eFuse row

◆ rowIdx

uint8_t EfuseRowWrite_t::rowIdx

Bit mask to apply to eFuse row data bits

◆ rsvd

uint8_t EfuseRowWrite_t::rsvd[3]

Index of eFuse row.