DP83869 PHY configuration parameters.
Data Fields | |
| bool | txClkShiftEn |
| bool | rxClkShiftEn |
| uint32_t | txDelayInPs |
| uint32_t | rxDelayInPs |
| uint8_t | txFifoDepth |
| uint32_t | idleCntThresh |
| uint32_t | impedanceInMilliOhms |
| Dp83869_Gpio0Mode | gpio0Mode |
| Dp83869_Gpio1Mode | gpio1Mode |
| Dp83869_LedMode | ledMode [DP83869_LED_NUM] |
| bool Dp83869_Cfg::txClkShiftEn |
Enable TX clock shift
| bool Dp83869_Cfg::rxClkShiftEn |
Enable RX clock shift
| uint32_t Dp83869_Cfg::txDelayInPs |
TX delay value
| uint32_t Dp83869_Cfg::rxDelayInPs |
RX delay value
| uint8_t Dp83869_Cfg::txFifoDepth |
TX FIFO depth
| uint32_t Dp83869_Cfg::idleCntThresh |
Viterbi detector idle count threshold
| uint32_t Dp83869_Cfg::impedanceInMilliOhms |
Output impedance in milli-ohms. Ranging from 35 to 70 ohms in steps of 1.129 ohms
| Dp83869_Gpio0Mode Dp83869_Cfg::gpio0Mode |
Mux mode of the GPIO_0 pin
| Dp83869_Gpio1Mode Dp83869_Cfg::gpio1Mode |
Mux mode of the GPIO_1 pin
| Dp83869_LedMode Dp83869_Cfg::ledMode[DP83869_LED_NUM] |
LED mode (source) configuration