FIFO related statistics of a MAC port.
Data Fields | |
| uint32_t | rxThroughputRate |
| uint32_t | txStartWords |
| uint32_t | txMaxBlocks |
| uint32_t | rxMaxBlocks |
| uint32_t | txBlockCount |
| uint32_t | rxExpressBlockCount |
| uint32_t | rxPreemptBlockCount |
| bool | txActiveFifo [ENET_PRI_NUM] |
| uint32_t CpswMacPort_FifoStats::rxThroughputRate |
Max throughput of the Ethernet ports to the crossbar SCR
| uint32_t CpswMacPort_FifoStats::txStartWords |
Number of 32-byte packet words in an Ethernet port transmit FIFO before packet egress will begin
| uint32_t CpswMacPort_FifoStats::txMaxBlocks |
Max number of blocks allowed on all TX FIFO priorities combined
| uint32_t CpswMacPort_FifoStats::rxMaxBlocks |
Max number of blocks allowed on the express and preempt RX FIFOs combined
| uint32_t CpswMacPort_FifoStats::txBlockCount |
Number of blocks allocated to the FIFO logical TX queues
| uint32_t CpswMacPort_FifoStats::rxExpressBlockCount |
Number of blocks allocated to the FIFO express RX queue
| uint32_t CpswMacPort_FifoStats::rxPreemptBlockCount |
Number of blocks allocated to the FIFO preempt RX queue
| bool CpswMacPort_FifoStats::txActiveFifo[ENET_PRI_NUM] |
Whether a FIFO priority has one or more queued packets or not