EST timestamping configuration parameters.
Data Fields | |
| Enet_MacPort | macPort |
| CpswMacPort_EstTimestampMode | mode |
| uint8_t | priority |
| uint8_t | domain |
| Enet_MacPort CpswMacPort_EstTimestampCfg::macPort |
Port number.
| CpswMacPort_EstTimestampMode CpswMacPort_EstTimestampCfg::mode |
Timestamping mode. Determines what packets are timestamped.
| uint8_t CpswMacPort_EstTimestampCfg::priority |
Priority that timestamps will be generated on. Applicable for CPSW_MACPORT_EST_TIMESTAMP_ONEPRI and CPSW_MACPORT_EST_TIMESTAMP_FIRST_ONEPRI.
| uint8_t CpswMacPort_EstTimestampCfg::domain |
CPTS EST timestamp domain. It can be used to indicate and identify that an event came from EST.