Host port module configuration parameters.
Data Fields | |
| Enet_CrcType | crcType |
| bool | removeCrc |
| bool | padShortPacket |
| bool | passCrcErrors |
| uint32_t | rxMtu |
| bool | passPriorityTaggedUnchanged |
| bool | txCsumOffloadEn |
| bool | rxCsumOffloadEn |
| bool | rxVlanRemapEn |
| bool | rxDscpIPv4RemapEn |
| bool | rxDscpIPv6RemapEn |
| EnetPort_VlanCfg | vlanCfg |
| EnetHostPort_IngressPriorityType | rxPriorityType |
| EnetPort_EgressPriorityType | txPriorityType |
| Enet_CrcType CpswHostPort_Cfg::crcType |
Type of CRC on all port 0 egress, regardless of the CRC type in Ethernet port ingress
| bool CpswHostPort_Cfg::removeCrc |
Whether or not CRC is removed on port 0 egress
| bool CpswHostPort_Cfg::padShortPacket |
Whether short packets (ingress) are padded to 64-bytes or dropped
| bool CpswHostPort_Cfg::passCrcErrors |
Whether packets with CRC errors (ingress) are dropped or transferred to the destination ports
| uint32_t CpswHostPort_Cfg::rxMtu |
Max length of a received frame on ingress, including VLAN
| bool CpswHostPort_Cfg::passPriorityTaggedUnchanged |
Whether priority tagged packets should be passed unchanged (if set to true) or replaced with port's VID (if set to false)
| bool CpswHostPort_Cfg::txCsumOffloadEn |
Enable Tx checksum offload feature which allows TCP checksum computation to be offloaded to the CPSW for frames transmitted by any core. The Protocol specific info needs to be populated in the descriptor to indicate the location in the packet where the computed checksum should be inserted. On AM243x and AM64x platforms there is no specific control along Rx or Tx direction. Hence txCsumOffloadEn enables both Tx and Rx Checksum offload.
| bool CpswHostPort_Cfg::rxCsumOffloadEn |
Enable Rx checksum offload feature which allows TCP/UDP checksum validation to be offloaded to the CPSW for frames received. On AM243x and AM64x platforms this field has no meaning.
| bool CpswHostPort_Cfg::rxVlanRemapEn |
RX VLAN remap controls whether the hardware switch priority for VLAN tagged or priority tagged packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP (remap enabled)
| bool CpswHostPort_Cfg::rxDscpIPv4RemapEn |
RX DSCP IPv4 remap controls whether the hardware switch priority for IPv4 packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP (remap enabled)
| bool CpswHostPort_Cfg::rxDscpIPv6RemapEn |
RX DSCP IPv6 remap controls whether the hardware switch priority for IPv6 packets is determined from CPPI thread number (remap disabled) or via ENET_HOSTPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP (remap enabled)
| EnetPort_VlanCfg CpswHostPort_Cfg::vlanCfg |
Port VLAN configuration
| EnetHostPort_IngressPriorityType CpswHostPort_Cfg::rxPriorityType |
Ingress priority type
| EnetPort_EgressPriorityType CpswHostPort_Cfg::txPriorityType |
Egress priority type