Input args for CPSW_CPTS_IOCTL_SET_GENF and CPSW_CPTS_IOCTL_SET_ESTF commands.
Data Fields | |
| uint32_t | index |
| uint32_t | length |
| uint64_t | compare |
| bool | polarityInv |
| uint64_t | ppmVal |
| CpswCpts_FxnGenAdjDir | ppmDir |
| EnetTimeSync_AdjMode | ppmMode |
| uint32_t CpswCpts_SetFxnGenInArgs::index |
Function generator instance index value
| uint32_t CpswCpts_SetFxnGenInArgs::length |
Function generator length value
| uint64_t CpswCpts_SetFxnGenInArgs::compare |
64-bit function generator compare value
| bool CpswCpts_SetFxnGenInArgs::polarityInv |
Function generator polarity inversion flag true : Output of function generator asserts high false: Output of function generator asserts low
| uint64_t CpswCpts_SetFxnGenInArgs::ppmVal |
Function generator parts-per-million value
| CpswCpts_FxnGenAdjDir CpswCpts_SetFxnGenInArgs::ppmDir |
Direction of parts-per-million correction value
| EnetTimeSync_AdjMode CpswCpts_SetFxnGenInArgs::ppmMode |
Mode of correction value for GENF PPM: parts-per-million or parts-per-hour. If the ppmMode is set to CPSW_CPTS_PPM_DISABLE, the ppm value will be set to zero.