CPTS EST timestamp.
Data Fields | |
| uint64_t | tsVal |
| uint8_t | priority |
| uint32_t | seqNum |
| uint32_t | ingressPort |
| uint32_t | egressPort |
| uint32_t | domain |
| uint64_t CpswCpts_EstEvent::tsVal |
Time stamp value when the event occurred
| uint8_t CpswCpts_EstEvent::priority |
Hardware switch priority
| uint32_t CpswCpts_EstEvent::seqNum |
Sequence number of the event
| uint32_t CpswCpts_EstEvent::ingressPort |
Packet receive port number
| uint32_t CpswCpts_EstEvent::egressPort |
Transmit port number
| uint32_t CpswCpts_EstEvent::domain |
Domain number of the event