Unicast entry type info apart from MAC address that can be set.
Data Fields | |
| uint32_t | portNum |
| bool | blocked |
| bool | secure |
| bool | super |
| bool | ageable |
| bool | trunk |
| uint32_t CpswAle_UcastEntryInfo::portNum |
Port number that the packet with a unicast destination address is forwarded to
| bool CpswAle_UcastEntryInfo::blocked |
Indicates that packet with a matching source or destination address should be dropped
| bool CpswAle_UcastEntryInfo::secure |
Indicates that packet with a matching source address should be dropped, if the received port number is not equal to the port number in the table entry
| bool CpswAle_UcastEntryInfo::super |
Indicates that this address can be received in port state other than Forwarding state
| bool CpswAle_UcastEntryInfo::ageable |
Indicates if the unicast entry is subject to aging
| bool CpswAle_UcastEntryInfo::trunk |
Indicates if the portNum refers to trunk number of port number