Input args for CPSW_ALE_IOCTL_SET_TRUNK_CFG command.
Data Fields | |
| uint32_t | trunkId |
| uint32_t | numPorts |
| uint32_t | trunkPortIdx [CPSW_ALE_NUM_PORTS] |
| uint32_t | trunkHashBase |
| bool | dstIPEn |
| bool | srcIPEn |
| bool | innerVlanEn |
| bool | enablePri |
| bool | srcEn |
| bool | dstEnEn |
| uint32_t CpswAle_TrunkCfg::trunkId |
Trunk group ID value
| uint32_t CpswAle_TrunkCfg::numPorts |
Number of ports in the trunk group
| uint32_t CpswAle_TrunkCfg::trunkPortIdx[CPSW_ALE_NUM_PORTS] |
Trunk group index value
| uint32_t CpswAle_TrunkCfg::trunkHashBase |
Hash formula starting value
| bool CpswAle_TrunkCfg::dstIPEn |
Enables the destination MAC address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination
| bool CpswAle_TrunkCfg::srcIPEn |
Enables the source MAC address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination
| bool CpswAle_TrunkCfg::innerVlanEn |
Enables the inner VLAN ID value (C-VLANID) to be used with the hash function G(X) = 1 + X+ X^3 and affects the trunk port transmit link determination
| bool CpswAle_TrunkCfg::enablePri |
Enables the VLAN Priority bits to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination
| bool CpswAle_TrunkCfg::srcEn |
Enables the source IP address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination
| bool CpswAle_TrunkCfg::dstEnEn |
Enables the destination IP address to be used with the hash function G(X) = 1 + X + X^3 and affects the trunk port transmit link determination