Input args for CPSW_ALE_IOCTL_SET_POLICER_THREADCFG command.
Configuration to set the thread/flow id associated with a classifier.
Data Fields | |
| CpswAle_PolicerMatchParams | policerMatch |
| bool | threadIdEn |
| uint32_t | threadId |
| CpswAle_PolicerMatchParams CpswAle_SetPolicerThreadCfgInArgs::policerMatch |
Policer match config
| bool CpswAle_SetPolicerThreadCfgInArgs::threadIdEn |
Enable/disable thread id setting for this policer entry
| uint32_t CpswAle_SetPolicerThreadCfgInArgs::threadId |
Thread Id which will be enabled for this policer match