Input args for CPSW_ALE_IOCTL_SET_POLICER command.
Data Fields | |
| CpswAle_PolicerMatchParams | policerMatch |
| bool | threadIdEn |
| uint32_t | threadId |
| uint32_t | peakRateInBitsPerSec |
| uint32_t | commitRateInBitsPerSec |
| CpswAle_PolicerMatchParams CpswAle_SetPolicerEntryInArgs::policerMatch |
Policer match config
| bool CpswAle_SetPolicerEntryInArgs::threadIdEn |
Enable threadid setting for this policer entry
| uint32_t CpswAle_SetPolicerEntryInArgs::threadId |
Thread Id which will be enabled for this policer match
| uint32_t CpswAle_SetPolicerEntryInArgs::peakRateInBitsPerSec |
Peak rate in bits per second. 0 indicates rate limit is disabled
| uint32_t CpswAle_SetPolicerEntryInArgs::commitRateInBitsPerSec |
Commit rate in bits per second. 0 indicates rate limit is disabled