Input args for CPSW_ALE_IOCTL_SET_PORT_MIRROR_CFG command.
Data Fields | |
| bool | srcEn |
| bool | dstEnEn |
| bool | matchEn |
| uint32_t | dstPortNum |
| uint32_t | toPortNum |
| CpswAle_MirrorMatchParams | matchParams |
| uint32_t | srcPortNumMask |
| bool CpswAle_PortMirroringCfg::srcEn |
Enables the source port mirror option. When this bit is set any port with the pX_mirror_sp set in the ALE Port Control registers set will have its received traffic also sent to the mirror_top port
| bool CpswAle_PortMirroringCfg::dstEnEn |
Enables the destination port mirror option. When this bit is set any traffic destined for the mirror_dp port will have its transmit traffic also sent to the mirror_top port
| bool CpswAle_PortMirroringCfg::matchEn |
Enables the match mirror option. When this bit is set any traffic whose destination, source, VLAN or OUI matches the mirror_midx entry index will have that traffic also sent to the mirror_top port
| uint32_t CpswAle_PortMirroringCfg::dstPortNum |
The port to which destination traffic destined will be duplicated
| uint32_t CpswAle_PortMirroringCfg::toPortNum |
The destination port for the mirror traffic
| CpswAle_MirrorMatchParams CpswAle_PortMirroringCfg::matchParams |
ALE lookup table entry info that when a match occurs will cause this traffic to be mirrored to the mirror_top port. Must be valid if matchEn is TRUE
| uint32_t CpswAle_PortMirroringCfg::srcPortNumMask |
Source port number mirroring enable bitmask