Output args for CPSW_ALE_IOCTL_GET_POLICER, CPSW_ALE_IOCTL_SET_POLICER_THREADCFG, CPSW_ALE_IOCTL_BLOCK_CLASSIFIER_HOSTPORT and CPSW_ALE_IOCTL_SET_INTERVLAN_CFG commands.
Data Fields | |
| uint32_t | policerMatchEnMask |
| uint32_t | port |
| bool | portIsTrunk |
| uint32_t | priority |
| uint32_t | ouiAleEntryIdx |
| uint32_t | srcMacAleEntryIdx |
| uint32_t | dstMacAleEntryIdx |
| uint32_t | ivlanAleEntryIdx |
| uint32_t | ovlanAleEntryIdx |
| uint32_t | etherTypeAleEntryIdx |
| uint32_t | srcIpAleEntryIdx |
| uint32_t | dstIpAleEntryIdx |
| bool | threadIdEn |
| uint32_t | threadId |
| uint32_t | peakRateInBitsPerSec |
| uint32_t | commitRateInBitsPerSec |
| uint32_t | policerEntryIdx |
| bool | egressOpEn |
| uint32_t | egressOpcode |
| bool | ttlCheckEn |
| uint32_t | egressTrunkIdx |
| uint32_t | dstPortMask |
| uint32_t CpswAle_PolicerEntryOutArgs::policerMatchEnMask |
Bitmask selecting classifier types to be enabled for this policer.
| uint32_t CpswAle_PolicerEntryOutArgs::port |
Port number to match. Valid if bit CPSW_ALE_POLICER_MATCH_PORT in policerMatchEnMask is set
| bool CpswAle_PolicerEntryOutArgs::portIsTrunk |
Flag indicating port number is a trunk group. Valid if bit CPSW_ALE_POLICER_MATCH_PORT in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::priority |
Received packet priority to match. Valid if bit CPSW_ALE_POLICER_MATCH_PRIORITY in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::ouiAleEntryIdx |
OUI ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OUI in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::srcMacAleEntryIdx |
MAC address ALE table entry index to match source MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACSRC in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::dstMacAleEntryIdx |
MAC address ALE table entry index to match destination MAC address. Valid if bit CPSW_ALE_POLICER_MATCH_MACDST in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::ivlanAleEntryIdx |
Inner VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_IVLAN in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::ovlanAleEntryIdx |
Outer VLAN ALE table entry index to match. Valid if bit CPSW_ALE_POLICER_MATCH_OVLAN in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::etherTypeAleEntryIdx |
EtherType ALE table entry index to match. It's valid if bit CPSW_ALE_POLICER_MATCH_ETHERTYPE in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::srcIpAleEntryIdx |
IP address ALE table entry index to match as source IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPSRC in policerMatchEnMask is set
| uint32_t CpswAle_PolicerEntryOutArgs::dstIpAleEntryIdx |
IP address ALE table entry index to match as destination IP address. Valid if bit CPSW_ALE_POLICER_MATCH_IPDST in policerMatchEnMask is set
| bool CpswAle_PolicerEntryOutArgs::threadIdEn |
Flag indicating if thread id setting is enabled for this policer entry
| uint32_t CpswAle_PolicerEntryOutArgs::threadId |
Thread Id which will be enabled for this policer match. Valid if threadIdEn is true.
| uint32_t CpswAle_PolicerEntryOutArgs::peakRateInBitsPerSec |
Peak rate in bits per second. 0 indicates rate limit is disabled
| uint32_t CpswAle_PolicerEntryOutArgs::commitRateInBitsPerSec |
Commit rate in bits per second. 0 indicates rate limit is disabled
| uint32_t CpswAle_PolicerEntryOutArgs::policerEntryIdx |
ALE policer table entry index
| bool CpswAle_PolicerEntryOutArgs::egressOpEn |
Egress Op enabled
| uint32_t CpswAle_PolicerEntryOutArgs::egressOpcode |
Egress Op code:
| bool CpswAle_PolicerEntryOutArgs::ttlCheckEn |
TTL check enabled for the interVLAN route. Valid only if egress op code has interVLan route enabled
| uint32_t CpswAle_PolicerEntryOutArgs::egressTrunkIdx |
Trunk index to be used if detPort for interVLAN route is a trunk. Valid only if egress op code has interVLAN route enabled
| uint32_t CpswAle_PolicerEntryOutArgs::dstPortMask |
Port mask to which the packet is to be routed. Valid only if egress op code has interVLAN route enabled